Skip to main content

Renesas Blog

The Virtual Turnkey Platform that Accelerates E/E Architecture Development Blog

The Virtual Turnkey Platform that Accelerates E/E Architecture Development

To easily develop large-scale and complicated E/E architectures, we provide a Virtual Platform (VPF) for software development without an actual device and a software development kit that runs on the VPF.

Renesas Virtual Development Environment for Fast Application SW Development

Multi-Core Debug and Trace Tool for R-Car S4

In this blog, the multi-core debug and trace tool for R-Car S4, which was released in April 2022, is introduced.

Main blog image

Renesas Commits to Meet ISO/SAE 21434, Road Vehicles Cybersecurity Engineering International Standard

Renesas is fully committed to meeting ISO/SAE 21434 for its automotive microcontrollers (MCUs) and system-on-chip (SoC) solutions effective with new developments from January 2022.

RX72M Wide Range blog thumbnail

RX72M Wide Range of Motor Control Applications via EtherCAT Communication

Effortlessly evaluate motor control via EtherCAT using provided hardware and software components.

True Wireless Stereo (TWS) Earbud Charger Cradle Blog

True Wireless Stereo (TWS) Earbud Charger Cradle

This is a highly integrated, yet modular and flexible, charger cradle, supporting independent power rails to recharge TWS earbuds and hearing-aids.

NIST Certifications and Tests Provide Security Solution Confidence

NIST Certifications and Tests Provide Security Solution Confidence

This blog looks at the importance of security certifications and explains how embedded developers can be assured that the heart of their product’s security works correctly.

e-AI x 3D Gesture Recognition How to use QE for Capacitive Touch

QE for Capacitive Touch Supports the Development of Gesture Applications using AI. Let’s check its ability!

QE for Capacitive Touch supports the development of gesture applications with the use of AI. This blog explains the creation and operation of the gesture and the recognition accuracy.

Main blog image

Data Science and Data Integrity within AIoT

The ever-growing abundance of data has led to the need to manage it in a way that ensures data quality by reducing duplication and guaranteeing the most accurate and timely outcome.

RZ/V2M blog image

Bid Farewell to ISP Tuning and Manual Parameter Tweaking with RZ/V2M "Tuned ISP"

Renesas’ "Tuned ISP" concept simplifies the ISP functions of the RZ/V2M MPU to speed up the image improvement process and shorten development time.

Learning at the Edge: Building Intelligence into the Industrial IoT Endpoint Blog

Learning at the Edge: Building Intelligence into the Industrial IoT Endpoint

IIoT endpoint devices are becoming increasingly intelligent with significant computing and AI capabilities at very low power at the endpoint, privacy and minimal bandwidth needs.