Skip to main content

RZ/T2H RZ/N2H Quick Start Guide: Linux and FSP

Jun 24, 2025

This video provides a complete walkthrough for setting up the RZ/T2H and RZ/N2H evaluation boards using the Linux Board Support Package (BSP). It covers everything from build procedures, board setup, and boot loader configuration to Software Development Kit (SDK) creation. The video also demonstrates running a sample program that combines Linux and real-time control using the Flexible Software Package (FSP), where Linux prints "Hello World!" while FSP on e² studio controls a blinking LED.

Chapter Titles

00:31 Environmental Requirements
01:24 Setting Up Environment
03:46 Boot Implementation
07:53 Example Implementation of Linux and FSP

Related Resources