Platform

    ※ The document for RZ/G2 is under preparation. For inquiries, please contact Renesas Electronics sales office or Contact US.

    Title Overview
    RZ/G2 Group Linux BSP Porting Guide (PDF) This guide explains how to port a RZ/G2 Linux BSP to a custom board based with a RZ/G2 group device.

    Hardware Manuals

    Title Overview
    RZ/G Series, 2nd Generation User's Manual: Hardware (ZIP) This is the user's manual for the RZ/G2 series of processors. The product line includes the RZ/G2H, RZ/G2M, RZ/G2N and RZ/G2E. Technical update can also be obtained together, so please read it in conjunction there.
    RZ/G2H Overview for User's Manual: Hardware (PDF) This is a overview of the hardware specification of the RZ/G2H processor.
    RZ/G2M Overview for User's Manual: Hardware (PDF) This is a overview of the hardware specification of the RZ/G2M processor.
    RZ/G2N Overview for User's Manual: Hardware (PDF) This is a overview of the hardware specification of the RZ/G2N processor.
    RZ/G2E Overview for User's Manual: Hardware (PDF) This is a overview of the hardware specification of the RZ/G2E processor.
    RZ/G Series User's Manual: Hardware (PDF) This is the user’s manual for the RZ/G-PF series of processors that are compatible with the RZ/G Linux Platform.
    The product line includes the RZ/G1H-PF, RZ/G1M-PF, RZ/G1N-PF, RZ/G1E-PF, and RZ/G1C-PF.
    Technical update can also be obtained together, so please read it in conjunction there.
    RZ/G1H-PF User's Manual & Technical Update These are the hardware specifications for the specific parts of the RZ/G1H-PF processor that support the RZ/G Linux Platform.
    Technical update can also be obtained together, so please read it in conjunction there.
    RZ/G1M-PF User's Manual & Technical Update These are the hardware specifications for the specific parts of the RZ/G1M-PF processor that support the RZ/G Linux Platform.
    Technical update can also be obtained together, so please read it in conjunction there.
    RZ/G1N-PF User's Manual & Technical Update These are the hardware specifications for the specific parts of the RZ/G1N-PF processor that support the RZ/G Linux Platform.
    Technical update can also be obtained together, so please read it in conjunction there.
    RZ/G1E-PF User's Manual & Technical Update These are the hardware specifications for the specific parts of the RZ/G1E-PF processor that support the RZ/G Linux Platform.
    Technical update can also be obtained together, so please read it in conjunction there.
    RZ/G1C-PF User's Manual & Technical Update There are the hardware specifications for the specific parts of the RZ/G1C-PF processor that support the RZ/G Linux Platform.
    Technical update can also be obtained together, so please read it in conjunction there.

    Verified Linux packages

    Title Overview
    Linux Interface Specification Yocto recipe Start-Up Guide (PDF) This manual explains how to build the Linux kernel for the RZ/G2 by using Yocto build system.
    RZ/G2 Group BSP Manual Set (ZIP) This is the set of user manuals that cover the driver module functions and interface specifications for controlling the hardware mounted on RZ/G2 products.
    RZ/G Verified Linux Package Start-Up Guide (PDF) Whole steps to use RZ/G Verified Linux Package on the reference board are described.
    Linux Interface Specificaiton Yocto recipe Start-Up Guide (PDF) This manual explains how to build the Linux kernel for the RZ/G1 by using Yocto build system.
    RZ/G1 Group BSP Manual Set (ZIP) This is the set of user manuals that cover the driver module functions and interface specifications for controlling the hardware mounted on RZ/G1 products.

    Application Notes/Other

    Title Overview
    RZ/G2 Group Application Note and Source Codes of Sample Applications (ZIP | English, 日本語) This application note introduces example applications that run on the RZ/G2 products.
    RZ/G Series Application Note (PDF) This application note introduces example applications that run on the RZ/G1 products.
    RZ/G Qt User Guide (PDF) About the open source version of Qt which is included in Verified Linux Package are described.
    RZ/G Linux Platform Customization Guide (PDF) How to change the items that are often customized with the RZ/G validated Linux package is described.
    RZ/G Linux Platform Developer's Guide (PDF) Development know-hows on RZ/G Verified Linux Package are described.