Categories: Development
A suite of application examples is available that demonstrates the functionality and operation of SSP frameworks, HAL drivers and modules.
The suite consists of standalone threaded applications using the ThreadX® RTOS to demonstrate the functionality of SSP frameworks, and standalone programs to exercise HAL drivers and modules. Framework examples interact with the SSP by calling the corresponding framework APIs while HAL drivers utilize the HAL driver APIs. Each application is called with a command-line interface on a serial terminal.
SSP developer examples can be run on all Synergy kits and reference designs. The SSP Developer Examples application note specifies which examples are supported for each kit.