Overview

The Renesas integrated development environment, or the High-performance Embedded Workshop, offers TargetServer (COM extension function) as the interface necessary to extend its functionality. This interface can be used to create customized windows for the High-performance Embedded Workshop, as well as build an environment in which to run the High-performance Embedded Workshop in cooperation with other applications.

Functions

TargetServer has various methods published at the Web site. These methods can be used to extend the functionality of the High-performance Embedded Workshop.

Composition

TargetServer (COM extension function) is comprised of the High-performance Embedded Workshop main body and TargetServer files (EcxHewTargetServer.dll and HewTargetServer.exe). Environments based on TargetServer (COM extension function) can be constructed by incorporating an interface on the user application side (*.exe and *.dll).

[General configuration]

[Example of the High-performance Embedded Workshop operating in cooperation with TargetServer]

Usage and a list of methods

To create customized windows for the High-performance Embedded Workshop, or to run it in cooperation with other applications, use Windows application development tools. At present, the methods listed below have been confirmed to operate normally in Visual C++ Ver.6.0 from Microsoft Corporation.

[List of TargetServer methods]

  • Execution control method
  • Register
  • S/W Break
  • Variable Break
  • Variable Trace
  • Interrupt
  • Download
  • Invoke/Quit
  • Workspace
  • Configuration/Session
  • Projects
  • Build
  • File
  • Coverage
  • Others

For details on how to use, refer to the TargetServer User's Manual included with the compiler package.

Sample Program

A sample program using TargetServer methods is supplied from Renesas. This sample program uses all of TargetServer methods. Use this sample program to understand how to use each method.

[Example program execution screen]

Information supporting development tools

Title Description
My Renesas Create a My Renesas account to use our tool download services, receive e-newsletter/update notifications, and take advantage of our other services.
e-learning Information for studying and learning about microcontrollers and microprocessors.
FAQ Frequently asked questions and useful hints for development.
Forum A forum and community site to share technical information, questions and opinions with others who use Renesas MCU's.
Tool News Tool release information and other important information.
Operating Environment Information on system requirements and operating environment for the latest version of tools.
Info on Discontinued Products A list of Renesas software and tools that have been discontinued and are no longer being offered for new projects.