メインコンテンツに移動

ブログ

What is Driving DDR5? Blog

What is Driving DDR5?

This blog goes over the need for faster and more memory and how DDR5 is addressing this need.

The RA MCU family is made to help solve your design challenges

The RA MCU Family is Made to Help Solve Your Design Challenges

The entry-level RA4E1 and RA6E1 MCUs address key design challenges including the optimal balance between performance and power consumption, as well as seamless migration options for future designs.

RA Book Features Blog

Get Where You’re Going with the Official Renesas RA Family Guide

This blog presents the RA Family Beginner’s Guide – A step-by-step guide that takes you from the basics of the FSP and RA toolchain to creating a project from scratch with the EK-RA6M4 evaluation kit.

Robotic Lawn Mower Blog

Lawn Maintenance Getting You Down? Robotic Mowers to the Rescue!

Compared to conventional lawn mowers, robotic lawn mowers offer many benefits including they are better for our environment and offer the convenience of remote programming, controlling and monitoring.

RapidCharge™ Controllers Prevent Fast Charger Hacking Blog

RapidCharge™ Controllers Prevent Fast Charger Hacking

Fast chargers and power supplies designed with Renesas' Rapid Charge™ controllers cannot be hacked, because they are hard-wired state machines that have no firmware that can be accessed and corrupted.

Ultimate optimization from custom ASICs

5 Things You May Not Know About an ASIC

There are many advantages to having an ASIC developed for your next product. Some of these advantages might be new to you. Here, we detail five of the lesser-known benefits.

ForgeFPGA

A New Era for Programmable Logic

There are many applications where a small amount of programmable logic can be useful, especially if the pricing is attractive. To address this gap, we have introduced a new line of low-density FPGAs.

Beacon blog

Beacon, Tag, or Both?

While the underlying technology is the same, the way beacons and tags are used is quite different, and understanding those differences leads to powerful new applications for consumers.

DA14586 Delivers Bluetooth 5 Spec Via the Smallest, Most-Flexible, Lowest-Power Chipset to Date Blog

DA14586 Delivers Bluetooth 5 Spec Via the Smallest, Most-Flexible, Lowest-Power Chipset to Date

With the market for IoT connectivity continuing to grow at a breakneck pace, it was only a matter of time before an even more efficient and performant Bluetooth® specification would come online.

GreenPAK in Action

3 Examples of GreenPAK in Action

See how GreenPAK ICs can be used for an analog clock motor driver, a basketball arcade machine, and a bike speedometer. These three applications are just the tip of the iceberg of what GreenPAK can do.