Skip to main content

Emulator Selection Guide for RH850 Family Microcontrollers

Jun 18, 2025

This video introduces emulators used in RH850 family microcontroller development. It covers the E2 emulator, an on-chip debug emulator, as well as the IE850A and IE850 full-spec emulators. A comparison table is included to help customers easily determine which emulator best suits their needs. Additionally, the extended functions of the E2 emulator are explained in detail.

Chapter Titles

00:00 Opening
01:21 Functional Comparison
02:32 CAN Communication Time Measurement Solution
03:53 External Trigger Input Function
04:06 External Trigger Output Function
04:22 Emulation Adapters
04:47 Web Page Introduction

Related Resources