Skip to main content

Renesas Blog

Protecting 'Highly Confidential Data' in IoT Devices (Part 2)

Protecting 'Highly Confidential Data' in IoT Devices (Part 2)

Learn how the Trusted Secure IP (TSIP) equipped RX microcontroller ensures the protection of confidential security parameters and personal data through its advanced 'Secure Key Storage' feature.

RZ/G2L series is the world’s first MPU certified PSA Certified Level 2

RZ/G2L series is the world’s first MPU certified PSA Certified Level 2.

RX Family Software – The Past and the Future and the Design of OTA Updating for RX MCUs via AWS/Azure

RX Family Software – The Past and the Future – #10 Design of OTA for RX MCU via AWS/Azure

Introducing the history and future of the software suite for the RX 32-bit MCU to enable development with low-code/no-code. The 10th blog is an introduction to firmware rewriting (OTA) of the RX family via AWS.

Low Voltage Motor Control with Enhanced Operation

Low Voltage Motor Control with Enhanced Operation

Reducing power consumption, physical size, and design costs are key challenges in the consumer appliance industry. Renesas offers a wide range of MCUs tailored for motor drive applications.

RZ/V Defect Detection in the Industrial Field

RZ/V Defect Detection in the Industrial Field

This article uses PCB defect detection as an example to introduce the structure of the YOLOv3-tiny defect detection AI algorithm, the deployment process, and inference performance in Renesas RZ MPUs.

RX26T new lineup expansion : Suitable for Motor Control Applications

RX26T New Lineup Expansion: Suitable for Motor Control Applications

We've released the RX26T (RAM48KB) product as a new addition to the RX26T group lineup. For those seeking a higher-performance and more advanced microcontroller for motor/inverter control, it is go-to choice.

Experience Digital Signal Processing  with RX MCU on the Cloud!

Experience Digital Signal Processing with RX MCU on the Cloud!

This blog introduces the RX Family DSP Solution on Lab on the Cloud, where you can connect to the RX microcontroller's evaluation board online and experience DSP firsthand

Renesas Powers a New Space Race

Renesas Powers a New Space Race

This blog discusses Renesas’ high-reliability (Hi-Rel) business, what’s driving the space race for Renesas, and what lies ahead.

<style type="text/css">@media (min-width: 996px) { .col-lg-7.first_blog_p { padding-left: 50px; }} @media (max-width: 995px) { .col-lg-7.first_blog_p { padding-top: 50px; }} </style> <div class="row"> <div class="col-lg-5" style="padding: 20px 20px 0px 20px;border: 1px solid #e1e0e0; border-radius: 4px;"> <h4>Radar Transceivers: Key Components for ADAS &amp; Autonomous Driving</h4>  <ul> 	<li><a data-entity-substitution="canonical" data-entity-type="node" data-entity-uuid="d18059ba-52f0-4c58-9978-db1070c9bd

How to connect the antennas?

At mmWaves the interfaces between the radar MMIC and the antennas need to be carefully designed to avoid any degradation on the system performance. This issue of the blog will highlight some aspects that need to be considered in the design of the transitions for different antenna configurations.

Configuration Issues with the RA6 Ethernet Controller

Configuration Issues with the RA6 Ethernet Controller

Are you having issues with the Ethernet controller on the RA6 MCU family? This blog suggests that you should check the configuration of the Arm® TrustZone® boundaries and explains why.