Skip to main content

Reprogramming RL78/G2x Code Flash Memory with Flash Driver SC [e2 studio]

May 28, 2025

This video demonstrates how to reprogram the RL78/G2x code flash memory using the Renesas Flash Driver RL78 Type 01 Smart Configurator version. It covers how to obtain and register the necessary components through Smart Configurator in e2 studio, as well as the essential project setup, settings, and debugging steps to reprogram the RL78/G2x code flash memory.

Chapter Titles

00:00 Opening
00:25 Creating a new project
01:05 Setting for the Smart Configurator
02:19 Setting for build 
03:20 Setting for debug
03:57 Debugging for the sample program

Related Resources