Skip to main content

RZ/G Software Package

Verified Linux Package

The Linux package packages the basic software required for the industrial field and provides it from Renesas as a software package that has been verified based on the data sheet.

Customers can use stable operating Linux + basic software and start application development immediately.

Traditionally, software provided by semiconductor manufacturers has not been systematically maintained. The software that makes up our Linux package has been verified and provided for maintenance. Significantly reduce customer software development load in embedded system development.

Key Features of the Verified Linux Package:

  • Super long-term support by Civil Infrastructure Platform™ (CIP™)
    • 5 years of backporting of additional functions for latest kernel
    • Over 10 years of security patch support
    • In addition, Renesas is independently carrying out activities to expand the scope of maintenance
  • Support for industry-standard APIs
  • Enhanced standard software components for use with industrial and IoT applications
    • Improved reliability, real-time performance, security, and functional safety as required by industrial segment
  • Support for industry-standard APIs
  • Free and simple click-through licensing
  • Free maintenance
Image
Renesas Verified Linux Package and Evaluation Board Kit

What is the Civil Infrastructure Platform (CIP)?

The Civil Infrastructure Platform is a platform that aims to establish a base layer for building Linux-based embedded systems that satisfy the requirements of modern civil infrastructure. It is driven by The Linux Foundation and global leading infrastructure system manufacturers.

Learn More

Licensing

A user agreement (free) with Renesas is required for using the RZ/G Linux package.

Trademark

Civil Infrastructure Platform and CIP are trademarks of The Linux Foundation in the United States and other countries.

Linux Package (VLP)

Renesas provides the basic software required for the industrial segment as the verified software package. Renesas also provides the multimedia package for installing H.264/H.265 Video codec and graphics (OpenGL ES) function into the RZ/G BSP (Board Support Package).
Please goto the page from the link that indicates the version of VLP in the table below, download the package and use it.

VLP VersionCIP Kernel VersionTarget DeviceVLP maintenance
end date*
RZ/G3SRZ/G2L,
RZ/G2LC,
RZ/G2UL
RZ/G2H,
RZ/G2M,
RZ/G2N,
RZ/G2E
RZ/G1H,
RZ/G1M,
RZ/G1N,
RZ/G1E,
RZ/G1C

VLP v3

5.10,
5.10-rt

check

check

check

check

2031/1H

VLP64

4.19,
4.19-rt

-

-

check

-

2029/1H

VLP v2

4.4,
4.4-rt

-

-

-

check

2027/1H

* Each VLP maintenance will be finished when the maintenance of corresponding CIP Linux Kernel version is completed.
   Use of the latest version VLP is recommended.
   Please refer to CIP Wiki for CIP Linux kernel maintenance periods.

Additional Packages for VLP

This software package runs on VLP.

HTML5 Package for Verified Linux Packages
HTML5 enables rich HMI development based on advanced Web technologies including JavaScript.

RZ MPU Security Package

  • RZ MPU Security Package
  • This package is to add Security functions (Secure Boot, Trusted Execution Environment, Hardware Cryptographic IP, Secure Debug, Security Configurator) to RZ MPU.

RZ/G Multi-OS Package

  • RZ/G Multi-OS Package
  • This package is the software package consisting of RZ/G Flexible Software Package (FSP) as software package for Renesas MCU with Arm® Cortex-M Core and OpenAMP as standardization API of framework for interprocessor communication for developing multi OS solution.

RZ/G AI Board Support Package


RZ/G Linux HMI Software Development Kit

The RZ/G HMI Software Development Kit (HMI SDK) provides a Linux HMI application development environment for the RZ/G Evaluation Board Kit (EVK). The HMI SDK is a one-package solution that includes necessary software for developing HMI application programs, such as Verified Linux Package (VLP), graphics library, video codec library, and HMI framework/libraries.

Advantages of HMI SDK

  • Easy-to-Use
    The HMI SDK provides a quick and easy development environment, lowering the barrier to entry for beginners to Linux to using a Linux MPU.
    • As long as you create a bootable SD card by using an image file in the SDK and put the SDK card on the board, an HMI demo starts on Linux.
    • You can start developing your application program easily since the SDK provides an installer for a toolchain of cross-development. And some application programs that run on HMI SDK Linux are available on our GitHub.
  • Free of Charge
    All software in the HMI SDK is available for free.
    • The HMI SDK consists of open-source software and libraries from Renesas, and they are provided for free.
    • As long as you have a supported RZ/G series EVK, you can start developing your HMI application program using the SDK.
  • Ready-to-Use
    The HMI SDK provides following GUI framework and libraries that are appropriate for HMI.
    • LVGL (Light and Versatile Graphics Library), which is a lightweight, free, open-source embedded graphics library. It does not use the GPU in the application program.
    • Chromium, which is a free and browser-based framework for application programs with GPU.

Target

The HMI SDK covers the EVK for RZ/G2L, RZ/G2LC and RZ/G2UL. In addition, we plan to expand support to other RZ/G series EVKs in the future.

For more details about the HMI SDK, please see:
https://renesas-rz.github.io/rzg_hmi_sdk/latest/


AOSP-based Package

The software package based on Android™ Open Source Project (AOSP) is a collection of the board support package (BSP) to run AOSP on RZ/G, the GPU middleware for graphic acceleration and the middleware for hardware video codecs.

Android VersionTarget MPU
RZ/G2LRZ/G2ERZ/G2NRZ/G2MRZ/G2H
Android 11 checkcheckcheckcheck
Android 12check check  
Android 13check check  

To use the Software Package based on Android Open Source Project, please contact your local sales representative or distributor.

Android is a trademark of Google LLC.

News & Blog Posts