Medium One, Inc.

Categories: Cloud Connection, Development

This partner project demonstrates that a Synergy kit can connect to the cloud and be remotely controlled with the use of the LED toggle feature.

The Synergy SK-S7G2 kit first tries to connect to an Ethernet then switches to Wi-Fi if Ethernet is unavailable. An interactive display built on the GUIX™ framework shows distance, duration and counter values obtained remotely from the cloud. The LED can be toggled either by pressing the button on the Synergy SK-S7G2 kit or on the Renesas IoT Sandbox web interface. Button presses are logged and sent to the cloud dashboard to remotely monitor the button state.

Features

This demo uses the Synergy SK-S7G2 Starter Kit and the AE-Wi-Fi application example kit to illustrate:

  • Remote monitoring and data transfer through a cloud platform
  • Interactive LCD display of cloud analytics, built with GUIX™
  • Unified onboarding and provisioning for both Ethernet and Wi-Fi (GT202)

Release Information

Copyright Disclaimer

© 2017 Medium One. All Rights Reserved.

The content included herein has been provided by other companies and Renesas does not claim any ownership therein. Renesas may or may not moderate or pre-screen the content included herein. Renesas requires partners to verify the functionality of their products on Synergy Platform and Renesas is not responsible in any way for the content included herein nor its quality. Renesas does not endorse any content included herein or any opinion, recommendation, or advice expressed therein, and Renesas expressly disclaims any and all liability in connection with such content, whether or not arising under the laws of copyright, libel, privacy, obscenity, or otherwise. Renesas does not provide support for any of this content; all support requirements should be directed to the owner or licensor of the content. Renesas retains the right, at its sole discretion and without prior notice, to pre-screen, refuse, or remove any content from the Synergy Platform.

Synergy Download

Medium One Cloud Agent for Synergy

1.16.11.03

Current Public Release

Release Date:2016-11-03

MCUs Supported: S7G2, S3A7

MD5: 832f6dc5c5fc32ffdc91d5283574a997

What's New?

First public release.    - Supports Smart Chef S3A7 Demo    - Supports Connected Weather SKS7 Demo

Installation Instructions

Please see the user’s manual for the Cloud Agent.

For the demo application, please refer to the Quick Start Guide: http://renesas-blog.mediumone.com/synergy-starter-kit-sk-s7g2-with-connected-weather-demo-quick-start-guide/