Skip to main content

New IDT Wireless Power Chipset Untethers Tablets and Phablets

The P9240 Transmitter and P9022A Receiver Bring Wireless Charging Capabilities to Medium-Sized Electronic Devices

February 26, 2015

SAN JOSE, Calif., Feb. 26, 2015-- Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today introduced a wireless power chipset designed to untether medium-sized electronic devices such as tablets and phablets. Complying with the Wireless Power Consortium (WPC) medium-power specification for magnetic induction charging, the P9240 transmitter and P9022A receiver operate together to deliver 10 W of power. The chips join the award-winning portfolio of IDT wireless power semiconductors already designed into smart phones, wearables, charging stations, furniture and accessories.

The P9240 is a highly compact transmitter supporting up to 15 W of power transfer. Featuring an integrated 32-bit ARM ® Cortex® M0 processor, the transmitter’s high level of integration means a minimal number of external components are required, reducing engineering efforts and board space. The chip is housed in a compact 5 millimeter by 5 millimeter package.

The P9022A is a 10 W wireless charging receiver that enables faster charging of tablets, phablets, and smart phones with large batteries. The integrated microcontroller provides flexible programmability and allows the use of all WPC-compliant medium-power receiver coils in end applications.  The P9022A receiver features an integrated synchronous full-bridge rectifier and a high-efficiency integrated synchronous buck converter.

“The wireless power ecosystem is growing rapidly as innovative design teams seek to cut through the tangle of cords needed to power our electronics,” said Arman Naghavi, IDT’s vice president of Analog Power Technology. “This new chipset brings IDT’s uniquely flexible, compact wireless power capabilities to this mid-power class of electronics.” 

The P9240 is a wide input range transmitter chipset with an integrated step-down regulator. It features low standby current that meets Energy Star standards; proprietary slew rate control drivers that deliver best-in-class metrics for electromagnetic interference, allowing OEMs pass CISPR22 Class B tests with several dB margin; and simultaneous voltage and current demodulation for more robust receiver to transmitter communication. The transmitter supports I2C, SPI and UART serial interfaces.

The P9022A receiver has proprietary back channel communication--a two-way communication protocol feature that enables users to tailor operating performance, identification and authentication. The chip also provides improved foreign object detection (FOD) for safety.

For more information, please contact an IDT sales representative.

About IDT Wireless Power

IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC), Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP) as a board member.  IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver, and the first dual-mode receiver IC compatible with both WPC and PMA standards. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.