Title | Type | Description | Company |
---|---|---|---|
Model-Based Development Environment for RH850, R-Car Family [Embedded Target for Virtual Platform] | Model-Based Development | Embedded Target for RH850 Virtual Platform is a development environment that generates peripheral code for target devices from Simulink® models and enables cooperative verification as Virtual Hardware In the Loop Simulation (vHILS) in a virtual environment with Simulink. | Renesas |
RH850 Multicore Model-Based Environment [Embedded Target for RH850 Multicore] | Model-Based Development | The Embedded Target for RH850 Multicore is a RH850 model-based multicore environment that simplifies complex driving control for the autonomous-driving era. In addition to the multicore support of the PILS tool for automatic configuration of environments, Embedded Target for Renesas CS+, it can also be interlinked with a model-based parallelization tool from eSOL Co., Ltd. | Renesas |
MBD Solution for RH850/C1M-Ax | Model-Based Development | The MBD solution for RH850/C1M-Ax connects the MCU peripheral IP model with the user model through an intuitive physical value interface and realizes seamless Model-Based Design (MBD) from simulation to embedding generated code into the actual hardware. | Renesas |
R-Car NAS (Neural Architecture Search) | Model-Based Development | Tool for automatically designing deep learning models that run efficiently on R-Car | Renesas |