FemtoClock™ 2 Evaluation Kit
This is the evaluation kit for the RC32514A and RC22514A. The board will come populated with an RC32514. The RC22514 is functionally a subset of the RC32514A, so this...
The RC32514A is a small, low-power timing component designed to be placed immediately adjacent to a PHY, switch, ASIC or FPGA that requires several reference clocks with jitter performance less than 100fs. The RC32514A can act as a frequency synthesizer to locally generate the reference clock, a jitter attenuator to perform local clean-up and/or frequency translation of a centrally-supplied reference, a synchronous Ethernet equipment clock to perform passband filtering and clean-up of network-supplied references or as a DCO for frequency margining or OTN clock applications. It contains an internal crystal which can be leveraged as the frequency reference for the onboard PLL if desired.
Software title
|
Software type
|
Company
|
---|---|---|
Renesas IC Toolbox (RICBox) The Renesas IC Toolbox (RICBox) software platform enables customers to configure Renesas devices on evaluation kits when attached to the computer running the software.
|
Software Package | Renesas |
1 item
|
This is the evaluation kit for the RC32514A and RC22514A. The board will come populated with an RC32514. The RC22514 is functionally a subset of the RC32514A, so this...
Schematic symbols, PCB footprints, and 3D CAD models from SamacSys can be found by clicking on products in the Product Options table. If a symbol or model isn't available, it can be requested directly from the website.
Demonstration of Renesas’ Lab on the Cloud virtual environment for FemtoClock®2 ultra-low phase noise synthesizer and jitter attenuator.
Blog Post | Apr 27, 2021 | ||
Blog Post | Jun 14, 2019 | ||
News | Dec 14, 2017 | ||
News | Jul 18, 2016 |