e-AI Failure Prediction Becomes Standard Operation

This demonstration shows that one Renesas MCU realizes motor control and fault detection for an application simultaneously. e-AI discovers an application fault through the abnormal state of motor. Abnormal state of motor is detected by the acceleration sensor, also by current, torque and rotation speed which are the information stored in the motor control MCU. e-AI makes motor control more intelligent, predicts the maintenance schedule, identifies the location of the failure, and realizes the endpoint in real time.

e-AI Failure Prediction Becomes Standard Operation

Added on 1月 16, 2019

e-AI demonstration for failure detection of motor drive / electronica 2018 (Munich, Germany)


Motor Failure Detection with e-AI

Added on 10月 02, 2018

This demonstration shows motor control and fault detection with a Renesas MCU.