Cost-efficient NCAP front camera based on Renesas R-Car V3M SoC

Hella Aglaia

Hella Aglaia shows an in-vehicle demonstration of a front camera based on the cost-efficient R-Car V3M for high volume production, using the heterogeneous hardware accelerators implemented in the SoC of Renesas Electronics. The field-proven application software demonstrates the recognition of vehicles and pedestrians. Other available features from Hella Aglaia include detection of Traffic Sign and Traffic Light, High Beam and Road Surfaces, and are available on the scalable R-Car V3M and R-Car V3H SoCs from Renesas.

Added on 2020-01-07

Hella Aglaia