Renesas packing is designed to protect semiconductors during transit and development.

Packing Types

Renesas Electronics has three packing types.

  Magazine Tray Tape
Packing Container Magazine/Packing Container Tray/Packing Container Tape/Packing Container
Packing Box Magazine/Packing Box Tray/Packing Box Tape/Packing Box

Packaging Label

The inner label example shown below applies to all products shipped since January 2012.

Label Example

Example Label

  Brevity code Description
SPN Booking parts number
PN Customer parts number
QTY Quantity
T・L・B Mounting condition(In special case)
MSL Moisture sensitivity levels (In special case)

(4) and (5) listed above are not labeled on all products. See elements for special conditions for details.

Handling Guide

Important! Users must read and understand the Handling Guide before opening semiconductor packing containers. Failure to properly handle the packing container increases the risk of system assembly defects and / or serious quality & reliability problems.

Detailed Handling Guide

Guarding Against Static Electricity

Guarding against static electricity means first of all stopping it from occurring, and then if it does, discharging it appropriately (rapid discharge of a semiconductor device may damage the device).

For this reason, it is important to curb friction-charged static electricity caused by vibration during transportation, and to ensure an appropriate environment for handling of semiconductor devices is maintained. The operator handling semiconductor devices must have appropriate knowledge about static electricity.

The following table outlines measures to take when packing semiconductor devices, as well as examples of general precautions.

Packing Type Guarding Against Static Electricity
Magazine Antistatic additive is applied to the surface of plastic magazines, except for magazines made of aluminum or plastic material milled with carbon. Electrically conductive trays (plastic material milled with carbon) are used.
Tray Electrically conductive trays (plastic material milled with carbon) are used.。
Moisture Barrier Bag Aluminum laminate bags with static electricity diffusion are used,
Tape Emboss taped products use static electricity diffusion carrier tapes and reels.

Re-Use / Recycling of Packing Container

Renesas is committed to preserving the environment. Please recycle the packing containers (e.g., trays), or send back to Renesas Electronics for reuse.