SAN JOSE, CA – Adesto Technologies (NASDAQ: IOTS) will share its latest technology developments at Arm TechCon, an annual technology event that showcases advances in Arm’s architecture—from silicon design and software development to platform security and IoT solutions.
Who:Adesto, a leading provider of innovative application-specific semiconductors and systems for the IoT era
What:Adesto will demonstrate its innovative custom ASIC and non-volatile memory (NVM) solutions in its booth #1020, including:
- The SmartEdge™ platform which provides a uniquely cost-effective way to integrate sensing, calibrating, controlling and communication functions into a single ASIC for edge computing, resulting in up to 75% less PCB area and power consumption, and 80% lower BOM cost
- The octal EcoXiP™ memory solution which removes barriers for mass market eXecute-in-Place (XiP) applications by delivering the best performance, power efficiency, and cost metrics
In addition, Adesto will be featured in sessions during the technical program:
- Adesto’s Chief Technology Officer Gideon Intrater will present: “Optimizing System Performance and Power in New MCU Architectures,” discussing new memory architectures that enable designers to meet performance/power requirements of emerging intelligent IoT devices.
- Silvaco experts will join Adesto and Arm in presenting: “Improving Memory on the Edge Using Octal Serial Flash Cache,” exploring options for increasing the program memory on a device without significantly increasing cost and power or limiting performance.
When:Arm TechCon will be held Oct. 16-18, 2018.
The Adesto session will be held at 9 a.m. on Tuesday, Oct. 16th
The Silvaco session will be held at 11:30 a.m. on Tuesday, Oct. 16th
Where:San Jose Convention Center, San Jose, CA; Adesto booth #1020
To schedule a demonstration or personal briefing, please email [email protected].
About Adesto
Adesto Technologies (NASDAQ:IOTS) is a leading provider of innovative application-specific semiconductors and systems for the IoT era. The company’s technology is used by more than 2,000 customers worldwide who are creating differentiated solutions across industrial, consumer, medical and communications markets. With its growing portfolio of high-value technologies, Adesto is helping its customers usher in the era of the Internet of Things.
Adesto Technologies and the Adesto logo are trademarks or registered trademarks of Adesto Technologies Corporation in the United States and other countries. Other company, product, and service names may be trademarks or service marks of others.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.