Facial Recognition and Classification Kiosk with RZ MPUs

Added on 6月 20, 2019

An RZ/A1H MPU performs facial recognition and classification to offer content targeting different demographics, while an RZ/G1 MPU fills the display with HD graphics, scrolling touch menus, and embedded video in this interactive advertising kiosk developed by a Renesas customer. This is one of six demos Renesas Electronics presented at the Embedded Vision Summit 2019 in Santa Clara, CA, highlighting the capabilities of RZ/A and RZ/G MPUs for low-power, high-performance machine vision systems.