Renesas Ushers in New Era of Industrial Motor Commutation with High-Accuracy Inductive Position Sensing

IPS2200 Delivers Total Stray-Field Immunity, Lower Weight, and Cost-Effective Design in a Thin Profile for Industrial Motors

24 Jun 2020

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, introduced the magnet-free IPS2200 inductive position sensor. Featuring high accuracy and speed, total stray field immunity, and efficient motor integration in a thin and lightweight form factor, the IPS2200 is ideal for use as an absolute position sensor in a wide range of industrial, medical, and robot applications. The sensor allows customers to cost effectively tailor sensor design for their applications and maximize the performance of the sensor’s accuracy.

“Inductive position sensing is changing the game for industrial motor commutation as demands for high accuracy, high efficiency, and cost efficiency increase, particularly for multi-pole pair motors and off-axis applications,” said Christian Wolf, Vice President, Automotive Sensor Business Division at Renesas. “With the IPS2200, we are excited to offer a solution that takes customers from concept to PCB layout, enabling them to design their own resolver replacement and achieve lighter, better performing motors for their industrial, robotic, consumer and medical applications. Moving forward, Renesas will also explore the inductive sensors for use in automotive applications.”

The IPS2200 is designed around the motor, allowing customers to match the number of sectors to pole pairs of the motor to maximize accuracy, accommodating both off-axis (through shaft and side shaft) and on-axis positioning. The magnet-free IPS2200 is up to 10x thinner and up to 100x lighter with up to 250 krpm electrical speeds compared with traditional resolvers. The sensor’s thin and light form factor and total stray field immunity enables easier motor integration and provides the standard materials required for customers to manufacture their own resolver replacement – reducing bill of materials costs. With its four- or six-wire operation, the IPS2200 provides up to 10x faster speeds and very low latency compared with resolver- or magnetic-based solutions.

Key features of the IPS2200 include:

  • Industrial qualified, with stable operation in harsh environments and -40° to +125° C ambient temperatures
  • Interface: Sin/cos single ended or differential
  • Voltage Supply: 3.3V ±10% or 5.0V ±10%
  • Rotational Speed: Up to 250.000 rpm (electrical)
  • Propagation delay: Programmable, <10µs
  • Sin/cos gain mismatch and offset compensation
  • Overvoltage, reverse polarity, short-circuit protected
  • Digital programming interface: I²C or SPI

In addition, Renesas offers off-the-shelf tools that can be used to create tailored and customized sensing elements, as well as custom tools that can achieve coil optimization sets within about 30 minutes.

The IPS2200 is Renesas’ first inductive position sensor for industrial markets, joining the company’s robust portfolio of devices for industrial motor commutation, which includes microcontrollers, power management, and drivers.

Availability

The IPS2200 is available now with prices starting at $4.22 USD per unit in 1,000-unit quantities. The IPS2200STKIT evaluation kit is also available now. (Pricing and availability subject to change).

For more information on the IPS2200, including technical documentation and tools, please visit www.idt.com/IPS2200.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.