Renesas Electronics Introduces Second Generation USB 3.0-SATA3 Bridge SoC With Reduced External Components

Utilizes High-Speed of USB 3.0 Storage and Significantly Reduces the Total Number of Components

06 Mar 2013

TOKYO, Japan, March 6, 2013 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the availability of its new SuperSpeed Universal Serial Bus (USB 3.0) to Serial ATA (SATA) Revision 3 [Note] bridge SoC (system on chip, part number µPD720231) that enables the reduction of the total BOM significantly. The µPD720231 enables effective multi-gigabit per second (Gbps) data transfer between a USB 3.0 host system and a SATA device used in widely adopted external USB hard drives and solid state drives (SSD).

USB 3.0 technology delivers more than 10 times the data transfer performance of the commonly used USB 2.0 peripheral interface. As the demand for media storage capacities and data transfer speed increases, the µPD720231 offers a fundamental building block to create an improved user experience for external USB storage.

Renesas Electronics has played a leading role both in defining USB standards and in developing USB technology. Renesas has enabled the USB 3.0 market by releasing the µPD720200 USB 3.0 host controller to mass production in June 2009. Since then, the company's lineup of USB 3.0 host controllers has been widely adopted by customers worldwide. Total shipments of these products have already exceeded 62 million units. In December 2009, the company also released a UASP driver that further enhances the data transfer for storage devices by improving the performance limit of the BOT (Bulk-Only Transfer) standard used by USB 2.0, making it possible for external storage devices to take advantage of the increased speed offered by the new USB 3.0 standard. To respond to the need for even faster data transfer performance necessary with the increased scale of the data in the storage device market, Renesas introduced the µPD720230 bridge SoC and confirmed USB-IF certification in 2011.

 

The new µPD720231 device was developed to respond to the need to reduce the number of components and to simplify printed circuit board (PCB) controller design.

 

Key features of the new µPD720231 SoC:

  • (1) Contributes to downsizing and power saving

    Through integration, the new µPD720231 USB 3.0-SATA3 bridge SoC has reduced the number of components by 40 percent compared with the number of other commercial devices with equal functions. The µPD720231 features an embedded voltage regulator and power-on reset circuit. The new product can store firmware in SATA devices such as hard discs and SSD and can also omit external serial flash ROM.

     

  • (2) Support for SATA Revision 3.0 enables 6 Gbps high-speed data transfer

    The µPD720231 USB 3.0-SATA3 bridge SoC supports SuperSpeed USB transfer speeds of up to 5 Gbps—as well as the SATA Revision 3.0 6 Gbps bit rate achieving maximum data transfer performance of USB 3.0. Thus, users can utilize actual USB 3.0 transfer rate, free from the transfer speed of the SATA side.

     

  • (3) Supports high-speed UASP protocol, independent of OS

    Renesas' free UASP driver runs not only on the Renesas µPD720200 USB 3.0 host controller and its follow-on products, the µPD720200A, µPD720201 and µPD720202, but also on major chip sets with an embedded USB 3.0 host controller, enabling higher data transfer speed on Windows XP/Vista/7. Renesas licenses this driver from MediaLogic,corp.

     

    The new µPD720231 device is compatible with Microsoft UASP drivers on Windows 8, and therefore does not depend on PC platform or OSs and can work in any major environment with higher data transfer speed by UASP.

     

  • (4) Seamless connectivity with proven Physical Layer (PHY) core

    Renesas' USB 3.0 host controllers have provided the de facto USB 3.0 connection for various peripherals. The new µPD720231 bridge adopts the same proven PHY core used in these host controllers, eliminating the unknown when connecting to USB 3.0 hosts.

     

  • (5) Supports optical disc drive by ATAPI command support

    The new µPD720231 device can control BD/DVD drives by supporting ATAPI command. It facilitates design of BD/DVD drives with USB interface.

     

Refer to the separate sheet for the main specifications of the µPD720231 USB 3.0 SATA3 SoC.

 

Availability

Mass production started in February 2013 and is expected to reach a scale of 500,000 units per month in June 2013. (Availability is subject to change without notice.)

 

[Note]: SATA (Serial ATA) is a storage interface specification that supports high-speed serial communication. It was developed for high data transfer rate with mass storage devices such as hard-disk drives..

(Remarks)

Windows is a registered trademark of Microsoft Corporation in the United States and other countries. SATA is an unregistered trademark of Serial ATA International Organization. Other product names and service names that appear in this press release are all trademarks or registered trademarks of their respective owners.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.