RL78/G1D Bluetooth LE Wireless Solution

Bluetooth Low Energy (LE) is a low energy mode of Bluetooth wireless technology that has an effect on power consumption especially for battery-operated applications. The attractive point of Bluetooth Low Energy lies in that it can operate while being connected to applications for smartphones and tablets. Renesas RL78/G1D Bluetooth LE Solutions provide smart connections with the lowest level of power consumption in the industry and can be used in applications such as healthcare and fitness devices, home electric appliances and RFID tags that use beacons to connect them with smartphones at low power consumption without wires.

Image
RL78/G1D Bluetooth LE Wireless Solution

Devices

RL78 16-bit Bluetooth LE MCU: R5F11Axxxxx

Renesas' RL78/G1D low power 16-bit microcontrollers (MCUs) support Bluetooth Low Energy and enable reliable connections with current consumption levels among the lowest in the industry. The chip incorporates a balun element and a filter. It is only required to connect the chip to an antenna. Reduction in the number of external components leads to reduction in labor required for design and quality control. It also supports the long-term product supply program.

Image
RL78/G1D IC

RL78/G1D Module: RY7011A0000DZ00

The RL78/G1D module contains the RL78/G1D 16-bit MCU, a 32MHz crystal resonator for the RF chip and an antenna, all in a compact 8.95mm x 13.35mm x 1.7mm module. The module inherits the functional pins of the RL78/G1D, so not only can it be used for modem configuration, but the strengths of the microcontroller can also be leverage for embedded configuration. This Bluetooth Low Energy module offers a good balance between size and the number of functional pins.

RL78/G1D and RL78/G1D Module Product Page

Image
RL78/G1D Module

 

H/W & Kits

RL78/G1D Evaluation Board: RTK0EN0001D01001BZ

The RL78/G1D evaluation board can be used to evaluate and develop applications for Renesas' RL78/G1D Bluetooth Low Energy solution. The board consists of an RL78/G1D module which can be plugged on to the development board and connected to an IDE for development and debugging. The development board can also work with a PC GUI tool for application level evaluation.

This evaluation board is best suited for the following purposes.

  • For evaluation of the Renesas' RL78/G1D microcontroller device
  • For operation evaluation of Bluetooth Low Energy
  • For use as a principle prototype

The Renesas RY7011 module can be evaluated with the following configuration.

Image
RL78/G1D Module Evaluation Board

RL78/G1D Evaluation Board Product Page

Image
RL78/G1D Evaluation Board

RL78/G1D BLE Module Expansion Board: RTKYRLG1D0B00000BJ

The RL78/G1D BLE Module Expansion Board (RTKYRLG1D0B00000BJ) is an evaluation board with a Pmod™ interface that incorporates the RL78/G1D module (RY7011A0000DZ00).

Build IoT Devices Such as Sensors with the RL78/G1D Module and a Host MCU

Image
RL78/G14 Fast Prototyping Board

It can connect to the RL78/G14 Fast Prototyping Board (RTK5RLG140C00000BJ) and can be used to evaluate BLE functions. Additionally, customers can use the RL78/G1D evaluation board to develop new BLE applications with a BLE system employing the RL78/G1D 16-bit microcontroller (MCU). Use the expansion board together with sensor devices to easily evaluate and develop IoT applications.

*Each board can be purchased from distributors.

RL78/G1D BLE Module Expansion Board Product Page

Image
RTKYRLG1D0B00000BJ RL78/G1D BLE Module Expansion Board

S/W & Tools

Bluetooth Low Energy Protocol Stack for RL78 Family

The Bluetooth Low Energy protocol stack is software required to operate the RL78/G1D IC. It supports modem configuration and embedded configuration. It can also adapt to custom profiles created by customers.

Renesas has prepared a dedicated "Beacon Stack" that reduces current consumption by 40% in beacon operation that constantly transmits radio waves. Renesas also provides sample programs as a reference for customers' program development.

Bluetooth Low Energy Protocol Stack Sample Program:

  • Virtual UART (custom Profile) spplication
    This is a sample program that realizes serial communication and wireless communication between embedded devices. It has a simple AT command execution function to control and set Bluetooth LE communication, thereby realizing virtual UART communication where characters are transmitted/received via Bluetooth LE communication.
    Image
    Virtual UART Application
  • HOGP ASCII text keyboard sample program
  • Pulse oximeter profile sample program
  • Host sample for (RL78/G14, RX113) sample program
  • Sensor application
Image
Bluetooth Low Energy Protocol Stack

Beacon Stack Sample Program:

A transmitter that transmits a small amount of data once every few milliseconds to several seconds within a radius of several tens of meters is called a beacon. This signal is used for watching terminals, indoor navigation, position detection, movement management of moving objects, coupon issuance, etc. Most beacon transmitters run on coin-type or small batteries. Since radio waves are always transmitted at regular intervals, it is required to consume as little power as possible.

The Bluetooth LE MCU RL78/G1D realizes low power consumption operation that is optimal for beacon terminals.

  • Basic operation sample program
  • Connecting and updating beacon data sample program

Multi-Hop Sample Program:

Multi-Hop uses a beacon stack for the advertising and scanning. Relay equipment executes both transmission and reception for Multi-Hop frame relay via the flooding method. It's possible to communicate data via more than one appliance. You can execute broadcasting a command (e.g. lighting control) and gathering data (e.g. sensor data) by using Multi-Hop. And, you can either select or not select security for prevention of eavesdropping and falsifying.

Image
Multi-Hop Operation

Renesas offers Bluetooth LE software solutions corresponding to a wide variety of application development. See the protocol stack product page for more information.

Bluetooth Low Energy Protocol Stack for RL78 Family Page

Image
Beacon Stack Sample Program

 

GUI Tool - Windows Application

Even if you are not familiar with Bluetooth Low Energy, you can easily conduct Bluetooth Low Energy communication using the GUI tool without writing a program. You can confirm the API execution procedure and the setting values for various parameters while actually conducting communication activities. Additionally, you can also develop a program smoothly while referring to the results (logs) of the operation check.

Download GUI Tool: Bluetooth® Low Energy Protocol Stack GUI Tool Rev.1.13 - Sample Code (ZIP | English, 日本語) (PDF + Windows application)

Image
Bluetooth Low Energy GUI Tools

 

GATTBrowser - iOS/Android Application

The GATTBrowser smartphone application can be downloaded from the Apple App Store and Google Play.

The GATTBrowser app is used to check Bluetooth Low Energy behavior. It can scan Bluetooth LE devices which are advertising in the vicinity and can perform GATT-based communication with the connected Bluetooth LE device. You can easily check the sample application behavior. GATTBrowser assists in the development of products that implement the Renesas RL78/G1D device and module.

Download GATTBrowser:

Image
GATTBrowser for iOS/Android Application with RL78/G1D
Image
GATTBrowser QR Codes

 

RenesasBLE - iOS/Android Application

The "RenesasBLE" iOS/Android application created by Renesas can be downloaded from the Apple App Store and Google Play. RenesasBLE operates in conjunction with sample programs so you can immediately experience Bluetooth Low Energy. You can download all the sample programs for Android, iOS and RL78/G1D and immediately link what you experienced to development.

Download RenesasBLE:

Image
RenesasBLE iOS/Android Application
Image
RenesasBLE QR Codes

 

QE for BLE - Development Assistance Tool

The QE for BLE (for RL78 Family) is a dedicated tool for developing embedded software in systems which support the Bluetooth Low Energy protocol stack. This solution toolkit runs in the e² studio integrated development environment (IDE). The combination of the e² studio and QE for BLE makes it easy to test the communications features of Renesas' RL78/G1D Bluetooth LE MCU, thus reducing development periods for products being placed on the market. It can also design and generate the custom profile.

Please refer to the QE for BLE: Development Assistance Tool for Bluetooth Low Energy page for more information.

QE for BLE: Development Assistance Tool for Bluetooth Low Energy Page

Image
QE for BLE (RX)

 

Applied Solutions

RL78 Quick Solutions

The RL78 Quick Solutions demonstrate how RL78 low power MCUs combined with Renesas' analog and power products can create high-performance solutions for a wide variety of applications. Quick Solutions for the Industrial IoT, infrastructure, healthcare, and home and office are fully developed reference designs with a user’s manual, application details, schematic, bill-of-materials (BOM), and source code/project files that enable you to develop these solutions quickly.

Solution Title Overview
Healthcare
Smart Medicine Box with BLE Build a solution for managing personal medication with the Smart Medicine Box with Bluetooth LE reference design featuring the RL78/G13 and RL78/G1D MCUs.
Smart Blood Pressure Monitor Build a solution for tracking blood pressure and other vitals with the Smart Blood Pressure Monitor reference design featuring the RL78/L1A and RL78/G1D MCUs.
Smart Body Fat Scale Build a solution for body composition management with the Smart Body Fat Scale reference design featuring the RL78/L1A and RL78/G1D MCUs.
Industrial IoT
Smart Moisture Sensor Build a solution for monitoring soil moisture with the Smart Moisture Sensor reference design featuring the RL78/G11 and RL78/G1D MCUs.
Home & Office
PowerPoint Presenter Build a solution for presentation control with the PowerPoint Presenter reference design featuring the RL78/G1D MCU.
Smart LED Build a solution for LED lighting control with the Smart LED reference design featuring the RL78/G1D MCU.
Smart Lock Build a solution for home security with the Smart Lock reference design featuring the RL78/G1D MCU.

Winning Combinations

Renesas also offers many compelling analog + power + embedded processing + connectivity "Winning Combinations".

Solution Title Overview
Healthcare
Personal Blood Glucose Monitor Renesas’ blood glucose monitor (BGM) design utilizes the high-performance RA2 MCU series. The high-performance ADC provides an optimal fit for BGM applications where precision is required. With the addition of the RL78/G1D module, the system can be easily extended to intelligent connections and control via mobile devices.
Diaper Odor Detector The combination of Renesas’ gas and humidity sensors, and RL78/G1D Bluetooth LE MCU, makes it easier to monitor diaper odors in real-time through any handy device. This design also includes the ISL9000A, a dual LDO with low noise, very high PSRR, and low IQ.
Biosensing with Wireless Charging and Bluetooth This solution enables the realization of a very compact system that supports wireless charging, collects data from multiple biosensors such as the very compact pulse oximeter sensor, and transfers it to a smartphone or cloud via Bluetooth LE wireless communication.
Building Automation
Air Quality Control for IoT Building Automation The ZMOD4410 gas sensor and HS300x humidity sensor family along with low power and high functionality RL78/G14 microcontroller and industry's lowest level current consumption RL78/G1D Bluetooth LE MCU enable users to sense the environment for gases, measure and improve air quality, and provide observations of goods during transport.
Voice/Face Recognition for Security Systems This solution utilizes a combination of voice and facial recognition to provide authorized entry. The solution is based on the powerful RZ/G2M MPU platform with 4K2K resolution and H.265 decode features to accelerate voice/face recognition speed.
Home Appliance
Refrigerator Odor Detector The combination of Renesas’ gas sensor, humidity sensor, and RL78/G14 MCU, enables users to detect gases in the refrigerator. The measured values of odor level, temperature and humidity can be monitored by handy device via Bluetooth LE wireless communication with the RL78/G1D module (RY7011).
Weather Station Solution This solution supports smart home systems, where a master unit (indoor unit) aggregates weather data (temperature, humidity, CO2 concentration) that is measured by a slave unit (outdoor unit). This data can then be sent wirelessly to the cloud, and accessed through a smartphone.

Bluetooth Low Energy Utilization Proposals

Renesas proposes the utilization of Bluetooth LE wireless communication in various scenes.

FAQ

Please refer to the Knowledge Base for FAQs on Bluetooth specifications, MCUs, modules, protocol stacks, development environments, qualification, and more.

Knowledge Base > Bluetooth Low Energy Page

select_allSoftware & Tool Pages

Title Type Description Company
e² studio IDE and Coding Tool Eclipse-based Renesas integrated development environment (IDE).
[Support MCU/MPU: RA, RE, RX, RL78, RH850, Renesas Synergy, RZ]
(Note: You need to install compiler separately as an additional software)
(Note: No separate e² studio installation required for RA FSP, this will be installed as part of the FSP with e² studio installer (Platform Installer) on GitHub.)
Renesas
Renesas Flash Programmer (Programming GUI) Programmer (Unit/SW) Flash memory programming software [Support MCU/MPU and devices: RA, RE, RX, RL78, RH850, Renesas Synergy, Power Management, Renesas USB Power Delivery Family, ICs for Motor Driver/Actuator Driver, V850, 78KR, 78K0] Renesas
Bluetooth® Low Energy Protocol Stack for RL78 Family Protocol Stack Bluetooth v4.2 certified protocol stack (Target device: RL78/G1D)
Renesas
QE for BLE: Development Assistance Tool for Bluetooth® Low Energy Solution Toolkit Debugging support tool that specializes in Bluetooth® Low Energy system development [Plugin for Renesas IDE "e2 studio"] [Support MCU/MPU: RA, RX, RL78] Renesas

printNews & Additional Resources