A buck-boost converter generates an output voltage either greater or less than the input voltage. The advantage of using a buck-boost solution is regulating the output voltage over the full power source voltage range. Buck-boost converter solutions usually have lower efficiency and a larger footprint than buck converter solutions.

descriptionドキュメント

printニュース&各種リソース

分類 日付
40V Multi-Output Isolated Topologies 基本ページ 2020年4月9日
Pulse Width Modulation 基本ページ 2020年4月9日
Linear vs. Switching Regulators 基本ページ 2020年3月30日