This article describes the technical details of Renesas' wafer-by-wafer low dose rate acceptance testing program for Renesas' radiation hardened products. It also discusses the design and construction details of the vault-type 60Co irradiator facility that supports these acceptance testing activities.

Introduction

The low dose rate ionizing dose response of semiconductors has become a key issue in space applications. Routine 60Co acceptance testing at a high dose rate has been demonstrated to be nonconservative for some technologies, and is increasingly being regarded as a classical accelerated test that has transitioned into a nonlinear range. The actual dose rate in space is many orders of magnitude below these acceptance testing levels. Renesas is addressing this changed market using a three-phase approach.

Phase 1

First, a low dose rate testing program of 13 selected legacy parts was initiated in 2009[1, 2]

and has now been concluded. These tests were performed in accordance with the MIL-STD-883 Test Method 1019.7 diagnostic protocol.

In all cases, the experimental matrix consisted of five samples irradiated at:

  • High dose rate with all pins grounded
  • High dose rate under bias
  • Low dose rate with all pins grounded
  • Low dose rate under bias and one control unit

The majority of the legacy parts being tested under this program are implemented in dielectrically isolated complementary bipolar processes. Two of the legacy Enhanced Low Dose Rate Sensitivity (ELDRS) tests were performed on HS26CxRH parts, which use junction-isolated (bulk) epi complementary metal-oxide semiconductor (CMOS) technology. All 13 tested parts completed 150krad(Si) at low dose rate and the test reports are available on the Renesas website[3].

Phase 2

In the second phase, all new development parts at the time (e.g., ISL70001SRH[4] and ISL7884xASRH[5]) were characterized at both high and low dose rate as a routine part of the product development. These highly integrated parts are an extension of Renesas' radiation hardness assured (RHA) product line and use a 0.6µm bulk BiCMOS power management process. Both parts were found to be ELDRS-free.

Phase 3

In the third and final phase, Renesas introduced wafer-by-wafer low dose rate acceptance testing as a complement to current high dose rate acceptance testing. To support this testing, a vault-type 60Co low dose rate irradiator was built at Renesas' Palm Bay location.

Next, we'll discuss the design and construction of this facility and the test methodologies to be used for acceptance testing work.

High Dose Rate Qualification Procedures

Current Renesas high dose rate total dose acceptance testing is performed on a wafer-by-wafer basis. This procedure provides RHA assurance at the wafer level, which is the most basic level of the IC fabrication process.

Following probe and die separation, sample die are selected at random from each wafer; the sample size is based on transistor count (4 die/wafer for chips with less than 4,000 transistors or 2 die/wafer for chips with greater than 4,000 transistors) as outlined in MIL-STD-883, TM 5005, Group E, Subgroup 2.

The samples are assembled and characterized using the production automated test equipment (ATE) and are then irradiated at a high dose rate to the maximum level specified in the applicable standard microcircuit drawing (SMD). The irradiation is performed under bias.

A second round of ATE testing is then performed at room temperature only. Any rejects in the sample fail the wafer.

High dose rate testing at Renesas' Palm Bay, Florida location has historically been performed using Gammacell 220 60Co irradiators. Initial low dose rate testing at Renesas was performed using a J. L. Shepherd and Associates model 484 research 60Co low dose irradiator, which is not suited to volume long-term testing. Low dose rate testing has also been performed on an outsourced basis at White Sands Missile Range SVAD (White Sands, NM).

An extension of the current high dose rate wafer acceptance procedure to the low dose rate regime is not straightforward. Current high dose rate tests are performed to a level of 300krad(Si), in nearly all cases, and such a test can be performed in an afternoon. An equivalent 300krad(Si) test at 0.01rad(Si)/s takes some 347 days.

The current low dose rate level of general interest to the user and research communities is in the 50krad(Si) to 100krad(Si) range. An initial decision was thus made to acceptance test all wafers to 50krad(Si) at low dose rate, which strikes a balance between total ionizing dose (TID) level, test duration and cost.

Note that all products will be acceptance tested at low dose rate, including not only bipolar and BiCMOS products that are considered to be an ELDRS risk, but CMOS parts as well.

Since the exposure time at 50krad(Si) at .01rad(Si)/s is some 60 days, roughly 40 tests must be run in parallel on average for current production volumes, requiring a large isodose test volume irradiator. Supporting this large number of parallel tests required extensive test automation, both from the scheduling and power supply control and sequencing standpoints.

To support the low dose rate wafer level RHA acceptance testing program, Renesas has completed the construction and activation of a vault-type 60Co irradiator and associated equipment and fixturing.

Low Dose Rate Irradiation Facility

Construction and activation of the Renesas Palm Bay, Florida low dose rate facility is complete. The prime contractor was Hopewell Designs, Inc. (5940 Gateway Drive, Alpharetta, GA 30004).

Figures 1-3 provide conceptual CAD drawings of the facility. The vault structure has 36” walls and a 48” roof, both constructed of high-density concrete. This shielding structure provides an estimated 10,000x reduction in dose rate measured at 11 feet from the pop-up source.

ELDERS Facility Floorplan

Figure 1. CAD drawing of low dose rate irradiator vault floor plan showing the vault and source, concentric fixturing, the labyrinth entrance and the adjacent control room. Doors are not shown for clarity. The inside dimensions of the vault are 15 feet x 15 feet (5m x 5m).

ELDERS Facility Room Layout

Figure 2. Conceptual CAD drawing (not to scale) of room layout showing the central "pop-up" 60Co source and the approximately spherical device under test (DUT) board mounting structure. The source has a lower storage position in a 12” welded stainless steel well below grade. The 36” concrete walls and 48” roof provide a 10,000x estimated reduction in outside exposure rate.

ELDERS Facility DUT Board Mounting

Figure 3. Conceptual CAD drawing of two segments of the DUT board mounting system. The board holders are arranged in a partial sphere surrounding the 60Co source. All DUT boards are enclosed in individual PbAl spectrum hardening boxes to filter out secondary radiation. Note that the final version of this design has four DUT boards per arm for a total DUT board capacity of 64.

The radiation source consists of 50 Curie (Cy) of 60Co radioisotope in an air-actuated aluminum "pop-up" pellet. The pellet is housed in a stainless steel tube, which is in turn centrally located in a 12” welded stainless steel well (Figure 2).

  • The recurved stainless steel tube minimizes radiation leakage while the source is in the "down" position.
  • The exposure rate inside the concrete vault with the source in the shielded (down) storage position is estimated at 0.1mR/hr.
  • Estimated exposure rate at the exterior of the vault is 0.45mR/hr while the irradiator is in operation.
  • The design field uniformity within the irradiator test volume is ±10%, while the calculated uniformity is ±2.5%.
  • The design dose rate is 0.01rad(Si)/s (10mrad(Si)/s) at the DUT board location.
  • The separate source pellet design greatly simplifies source replacement.

The DUT boards are supported on aluminum structures; the horizontal distance between the source and the board location is designed to be changed to maintain the required dose rate as the source loses activity. The DUT board fixturing (Figures 3, 7 and 8) is designed to accommodate 64 9” x 12” PC boards. All DUT boards are enclosed in a spectrum hardening PbAl box to filter out secondary radiation. The fixturing system approximates an isodose sphere centered on the source pellet and consists of 16 "wings" each supporting one PbAl box enclosing four DUT board holders. Design calculations indicate that a new 50 Curie source will result in a dose rate of .0097rad(Si)/s at 48”, while a 22.5Cy source (representative of a 50Cy source after 5 years of decay) will result in the same dose rate at 36”. Predicted total dose uncertainty was calculated at ±3% or better, depending on data collection tools. All irradiations are overtested by 3% to compensate for this uncertainty.

Safety

Operator safety is a key issue in the design of any irradiation facility. All doors have interlocks and position sensors, and the facility is operated entirely from the control room. Emergency stop buttons are provided, which will immediately drop the source into the shielding well. Loss of power or air pressure, actuation of an emergency stop button or any attempts to open any of the doors will drop the source and force the system into a safe state. All systems including biasing power supplies and control computers are operated from dedicated uninterruptible power supplies (UPS), with long-term power outages (recall we’re in a hurricane zone) handled by on-site Diesel power generating facilities.

Hopewell Designs has a long history of building reliable and robust systems. Figures 4 and 5 show images of the irradiation facility taken during construction, while Figure 6 shows the completed facility.

ELDERS Facility Site Excavation

Figure 4. Site excavation before pouring the vault foundation. The top of the source well is clearly visible to the left of image center. The PVC piping provides cable raceways between the vault and the Renesas Palm Bay Building 58 control room (right).

ELDERS Facility Walls View

Figure 5. View of wall forms before the second (wall) concrete pour. The labyrinth vault access architecture can be clearly seen.

ELDERS Facility Final External View

Figure 6. External view of the completed low dose rate irradiator.

ELDERS Facility Popup Source

Figure 7. View of "pop-up" source (center) and surrounding test racks. The vertical test board holders and their PbAl spectrum hardening filter boxes are shown. The holders are on rails and can be moved towards the centrally located source as it loses activity. The curvature of the DUT rack is not apparent as the rack is hidden by the PbAl box. The system supports 64 simultaneous tests.

ELDERS Facility PbAl Box

Figure 8. Internal view of a PbAl box and enclosed DUT board rack. The curvature of the test rack can be clearly seen; this curvature combines with the circular arrangement of the racks to generate an approximately spherical isodose profile at the DUT boards.

 

Operation

Control and scheduling of 64 two-month acceptance tests (maximum) in parallel while taking source activity into account would be problematic at best. The Hopewell irradiator design puts most operations under computer control. The operator continues to have full control over the system, but is able to focus on areas where expertise is most needed. The automated irradiator control system is based on the National Instruments LabVIEW environment. Features include automatic calibration and calibration report generation, dose rate calculation and source decay correction. The irradiator calibration procedure uses an ion chamber and electrometer and is fully automated.

The irradiator has 64 board positions available, each of which can have up to eight different power supply voltages. Control and tracking of exposure time, total dose and dose rate are vitally important. Each DUT board is uniquely identified by a bar-coded label which enables the control computer to track all boards while in the chamber. Each DUT board socket is verified as meeting the ELDRS irradiation diagram (SMD or internal specification) before each new lot is loaded, and DUT board supply currents are recorded before initiating irradiation.

Other capabilities are system status, system safety and interlock status, exposure status and source position. Exposure rate and distance are linked so that when one is changed, the other is calculated and updated. Exposure and time are also linked. When an exposure rate is specified, the system calculates a position, automatically compensating for source decay.

Products with multiple power supply requirements typically require individual power supply power-up and power-down sequences. A dedicated power supply control computer determines and controls the supply voltages and power sequencing for the individual board. The power supply control computer records voltages and currents to ensure correct system operation. Figures 7 and 8 show the centrally located "pop-up" 60Co source and DUT board fixturing detail.

Low Dose Rate Acceptance Testing Procedure

The Renesas low dose rate acceptance testing procedure is similar to the current high dose rate procedure. Four sample die are drawn from each probed wafer and are processed through the entire high-reliability Class V screening sequence. TM 5005 allows a sample size of 2 for parts with greater than 4,000 transistors, but as both biased and unbiased tests are performed, this would reduce the effective sample size to 1; hence, a uniform sample size of 4 is used for all products. The samples (2 die are biased and 2 die are grounded) are then irradiated to 50krad(Si) at 0.01rad(Si)/s. A second round of room temperature ATE testing is then performed, and any rejects fail the wafer.

It is important to note that all Renesas RHA parts will eventually be qualified using this procedure. This reflects the increased emphasis on low dose rate performance within our customer base and also reflects recent results[6, 7] suggesting low dose rate sensitivity in advanced shallow trench isolated CMOS processes. The existing high dose rate acceptance testing procedure will continue, with a decision point some three years in the future when the current Gammacell 220 will go out of dose rate specification.

As a part of the low dose rate qualification, Renesas will provide an enhanced data package that will accompany each shipment of QML class level V low dose rate qualified product. The data package will include an updated Radiation Effects Certificate of Compliance (C of C) for high and low dose rate testing. It will also provide high and low dose rate room temperature variables data for pre and post irradiation tests.

Wafer by Wafer Low Dose Rate Acceptance White Paper (PDF)

References

[1] N. W. van Vonno, L. G. Pearce, J. S. Gill, E. T. Thomson, and P. J. Chesley, "Low Dose Rate Testing Results of Legacy Renesas Products," presented at the 2010 Radiations et ses Effets sur Composants et Systemes (RADECS) Workshop, Längenfeld, Austria (September 2010).

[2] N. W. van Vonno, L. G. Pearce, J. S. Gill, E. T. Thomson, and P. J. Chesley, "Results of Low Dose Rate Testing of LegacyRenesasl Products," presented at the 2011 IEEE Radiation Effects Data Workshop (July 2011).

[3] ELDRS Test Reports

[4] N. W. van Vonno, L. G. Pearce, H. W. Satterfield, E. T. Thomson, A. P. Williams, T. E. Fobes, P. J. Chesley and J. S. Gill, "Total Dose and Single Event Testing of a Hardened Point of Load Regulator," 2010 IEEE Radiation Effects Data Workshop Record (2010).

[5] N. W. van Vonno, L. G. Pearce, G. M. Wood, J. D. White, E. T. Thomson, T. M. Bernard, P. Chesley and R. Hood, "Total Dose and Single Event Testing of a Hardened Single-Ended Current Mode PWM Controller," 2010 IEEE Radiation Effects Data Workshop Record (2010).

[6] S. T. Witczak, R. C. Lacoe, J. V. Osborn, J. M. Hutson and S. C. Moss, "Dose Rate Sensitivity of Modern nMOSFETs," IEEE Trans. Nuc. Sci., vol. 52, no. 6 (December 2005).

[7] A. H. Johnston, R. T. Swimm and T. F. Miyahira, "Low Dose Rate Effects in Shallow Trench Isolation Regions," IEEE Trans. Nuc. Sci., vol. 57, no. 6 (December 2010).

ELDRS Test Facility

Total Dose Reports

Wafer-by-wafer production testing qualification at both low (ELDRS) and high dose rate under biased and unbiased conditions.

Orion Over Earth Image

SEE Reports

Single-event effects (SEE) testing of radiation hardened devices to characterize their performance in a heavy ion environment.

Mars Rover Image

Neutron Reports

Testing to determine the sensitivity of a device to the displacement damage caused by a neutron environment.

ドキュメント

分類 タイトル 日時
カタログ PDF 5.02 MB
カタログ PDF 467 KB
ホワイトペーパー PDF 533 KB
3 items

ビデオ

Wafer by Wafer Low Dose Rate Acceptance Testing (ELDRS)

The low dose rate ionizing dose response of semiconductors has become a key issue in space applications. We are addressing this changed market by introducing wafer by wafer low dose rate acceptance testing as a complement to current high dose rate acceptance testing.

Transcript

Philip: Intersil's been in the space market for so long that some of our IC's are still operational on programs like Voyager 1. Longer than many of our competition has been in this business.

Josh: We have product on virtually every satellite, rocket, and shuttle launch that has gone from the U.S. and around the world since the beginning of space programs over 50 years ago. When the space program and satellites were first being launched, there were a variety of requirements that really just focused on high dose rate as a de facto standard for monitoring radiation performance of semiconductors in space. It was found that in space, in the actual space environment that low dose rate was more the actual exposure.

Nick: Low dose rate testing has turned into a really key aspect of space craft design. Because the actual radiation environment in space is low dose rate and is not high dose rate. High dose rate is a testing environment and not an actual natural environment. Certain parts that look very good at high dose rates degrade with amazing lupidity, orders and orders of magnitude worse at low dose rate. That is being addressed by establishing a much upgraded irradiator facility.

Arthur: When manufacturing was first approached with this request, we went out and started looking at what was available out in the market, to purchase a completed tool. And it turned out that there was really no completed product available.

Nick: There are a number of ways in which you can build an irradiator. The least expensive way of doing that is to build a concrete vault with very thick walls.

Arthur: In building the vault was quite a feat. There's an eight foot pipe that had to go into the ground, and it had to be level plumb to the pouring of over eight feet of being less than a quarter of an inch and it also had to be at the height of the final finish of the floor. Then, in order to make the room radiation safe, for all the employees in the surrounding area, the wall thicknesses had to range between four and five feet thick. The radiation source is comprised of 10 Curie pellets into what's called a rabbit, which is basically a pipe that goes up and down a rail. So whenever it's time to irradiate the product, there's a blast of air that blows this rabbit to the top of the irradiator and it mechanically gets locked in and the boards then begin their exposure time. The irradiator is a panoramic irradiator so, in other words, it's a globe and the board system is designed to form the boards around this imaginary globe. And because of that shape we're able to maintain a consistent dose rate across all boards that are loaded into each box and I'd be glad to show it to you but none of you have your Homeland Security approval to look at the tool.

Nick: Our testing facility can run 64 tests in parallel and given that these are two-month tests, we can accommodate well over 300 tests a year.

Josh: So wafer by wafer testing means that we select four random devices off each wafer, we package them up and we put them in the radiation chamber. And they have to come out and pass the SMD limits. If they don't pass the SMD limits, then that wafer gets scrapped. So it gives the customer a confidence level that the devices that we're shipping are rad hard.

Nick: The value to the customer of getting parts that have been through the low dose rate testing program is one of assured performance in the low dose rate environment.

Phillip: By Intersil having this radiation assurance program, where we have both high dose rate and low dose rate capability, that puts Intersil in a leadership position as well as a position to, you know, address this trend for the long haul. Today, customers are able to determine if a part has been radiation tested at a high dose rate level by the RH designation in our part numbering scheme. Going forward, a customer will be able to determine if it's been low dose rate tested by the designation of the EH letters. EH designation means both high dose rate as well as low dose rate testing. We currently plan on releasing all of our rad hard parts in an EH flow. We are also investing heavily in the space business to continue our leadership position. All new parts that have been developed, or will be developed, over the next year to two or three years will also be EH tested as well. On our website you will find information about our lose dose rate acceptance testing. You will find details on the flow, the irradiator itself, as well as the specific parts that are being tested and will be released on this EH flow. There is a very detailed white paper on the website.

Josh: Intersil has continued to make significant investment in our rad hard, new product development as shown by the number of new products that have rolled out over the past three or four years. Intersil was the first IC manufacturer to have in-house ELDRS test capability on a production level. This is a significant investment to put this capability in place and shows our commitment to the marketplace for our next generation of space products and satellite programs over the next 30 to 40 years.