This video shows the 5th European Renesas MCU Car Rally held on 28th February 2019 at the embedded world exhibition in Nuremberg, Germany.
The task of the student contest was to build a self-guided model car from a car kit based on the high-performance RX 32-bit microcontroller. The sensors in front are able to detect a white line on the track. The challenge was to optimize the hardware and software that auto drives the car along the white line on the track.
More than 30 teams with almost 200 students and their tutors from all over Europe participated in the challenge. It was a perfect opportunity for students to combine practical learning and fun!
More information: www.renesas.com/university
2019-11-19