Robotic Lawn Mower Blog

Lawn Maintenance Getting You Down? Robotic Mowers to the Rescue!

Compared to conventional lawn mowers, robotic lawn mowers offer many benefits including they are better for our environment and offer the convenience of remote programming, controlling and monitoring.

Easy-to-Start Automotive MCU Accelerates the Development Cycle

Easy-to-Start Automotive MCU Accelerates the Development Cycle

Introducing the Easy-to-Start automotive microcontroller series that are easy to use, easy to develop and easy to access for automotive, industrial and consumer applications.

Outdoor Air Quality: It’s Not Just About Urban Areas Blog

Outdoor Air Quality: It’s Not Just About Urban Areas

Learn about the importance of air quality to our health and the benefits of being able to monitor air quality, regardless of location, with Renesas’ ZMOD4510 outdoor air quality sensor.

No Porting Required! Real-Time OS Program Development that Even a Super Beginner Can Do Blog

No Porting Required! Real-Time OS Program Development that Even a Super Beginner Can Do

Introducing the real-time OS project creation function, which is an essential function for those who are using an embedded real-time OS.

Ethernet TSN Switch IP Core Evaluated by Conformance Testing Provided by Spirent Communications Blog

Ethernet TSN Switch IP Core Evaluated by Conformance Testing Provided by Spirent Communications

Ethernet TSN Switch IP Core is a high-quality IP core that has passed the conformance test provided by Spirent Communications; watch the video of the IP core evaluated by FPGA using Spirent Automotive C1.

A Tiny RX23E-A Board for Digital Load Cell Blog

A Tiny RX23E-A Board for Digital Load Cell

The RX23E-A, which integrates an MCU and high-precision Analog Front End on a single chip, is ideal for realizing integrated sensing and signal conditioning of a digital load cell in the same housing.

Condition Monitoring ASICs Extend Systems’ Lifetime Blog

Condition Monitoring ASICs Extend Systems’ Lifetime

With an ASIC solution, all the condition monitoring circuitry can be placed on the same chip with all the required electronics for the core function of the product.

The Art of Networking (Series 2): PCIe Goes Automotive Blog

The Art of Networking (Series 2): PCIe Goes Automotive

In this blog, we give a brief background summary of PCIe, what its potential PCIe use cases are and what needs to be looked at to smoothen the adaption path of PCIe in future automotive applications.

Easy Azure IoT Connection! RX65N 32-bit MCU Supports Azure RTOS Blog

Easy Azure IoT Connection! RX65N 32-bit MCU Supports Azure RTOS

The RX family of 32-bit MCUs offers evaluation kits with Azure Certified Device certification, sample code and IDE for deploying Azure RTOS. These enable easy connection to Azure IoT Hub.

FPGAマイコンH8SをFPGAに組み込もう

FPGAマイコンご紹介 ~FPGAにH8Sを組み込もう~

H8SをFPGAに組み込んだ実装例を元にFPGAマイコンをご紹介します。