Evolution of sensing equipment and force sensor measurement using RX23E-A

Evolution of Sensing Equipment and Force Sensor Measurement Using RX23E-A

A force sensor can be mounted to the tip of a robotic arm to measure load and torque. This blog introduces the Application Note on force sensing measurement using the RX23E-A 32-bit MCU.

Changes in Automotive E/E Architecture and Semiconductor Initiatives in the CASE+E Era

Japan IT Week特別講演「CASE+E時代における車載E/Eアーキテクチャの変化と半導体への取組み」

CASE+Eのこれからの自動車業界において半導体

に求められる価値提供、及び当社のアプローチをご紹介します。

RapidCharge™ Controllers Prevent Fast Charger Hacking Blog

RapidCharge™ Controllers Prevent Fast Charger Hacking

Fast chargers and power supplies designed with Renesas' Rapid Charge™ controllers cannot be hacked, because they are hard-wired state machines that have no firmware that can be accessed and corrupted.

Smart Glasses

A Wireless Charging Application for Wearable Tech Extended to Smart Glasses

Learn about the prototyping process and challenges encountered in the development of a next-generation wireless charging solution to address wearable tech.

RX - The Road Ahead!

RX - The Road Ahead!

For the RX MCU family, consumer and industrial applications will continue to be our primary focus in the next few years. We will also focus on IoT-related applications in these two areas.

Multi-Cell USB-PD + QC2 & QC3 Power Bank Blog

Multi-Cell USB-PD and PPS Power Bank with Qualcomm Quick Charge and OS Independent Monitoring

/node/1601921This is a detailed description of a solution for a multi-cell USB Power Delivery (USB-PD) enabled power bank using a 2S to 4S battery stack that supports USB-PD 3.0, PPS and Qualcomm Quick Charge.

The Art of Networking (Series 7): TSN in a Virtualized Environment

The Art of Networking (Series 7): TSN in a Virtualized Environment

Here, we show solutions for Precision Time Protocol (PTP) time distribution to virtualized OS with the help of hardware-assisted virtualization (Renesas R-Switch2) to solve challenges quickly.

Radar Transceivers: A Key Component for ADAS & Autonomous Driving - Blog 3: Radar Range: How Far Can a Radar “See”?

Radar Range: How Far Can a Radar “See”?

In the third entry of this series on automotive radar, we will analyze the factors which limit the range of detection of automotive radar and how they relate to the performance of the RF IC.

A Breath of Fresh Air: Battery Powered Air Quality Monitoring Blog

A Breath of Fresh Air: Battery Powered Air Quality Monitoring

Indoor air quality is important to our health and being able to monitor it with battery-operated devices using Renesas’ ZMOD4410 ultra-low power air quality sensor is beneficial.

SW Platform/Dev. Env. for E/E Architecture Series 11; Infrastructure - The Next Level of In-car Experience & Safety

We make the core software that drives the brain, the semiconductors, at the center of the increasingly highly featured and complex systems brought together through E/E architectures.