First Android 4.0 to Android 4.0 Handset Over The Air VoLTE Demonstration Contributes Various Rich Media Interactions

2012年7月19日

TOKYO, Japan, July 19 2012 — Renesas Mobile Corporation, a premier supplier of advanced cellular platforms, today announced that it has successfully demonstrated high definition Voice over LTE (VoLTE) and short messaging service (SMS) over the air with Nokia Siemens Networks, the world's specialist in mobile broadband. Conducted using Nokia Siemens Networks' commercially available infrastructure, this test represents the first over the air demonstration of calls to and from an Android 4.0 (Ice Cream Sandwich) based device using VoLTE. This technology milestone sets the scene for operators to migrate to providing all their services over IP, including voice and SMS, thereby freeing up legacy circuit switched GSM and WCDMA cellular networks.

Renesas Mobile reference devices running Android 4.0 and based on the Renesas Mobile SP2531 modem platform with VoLTE integrated were used for the demonstration. The device connected with Nokia Siemens Networks' LTE radio network, Evolved Packet Core (EPC) and IP Multimedia System (IMS) to receive and transmit high definition VoLTE and SMS traffic. The Nokia Siemens Networks implementation meets GSMA ir.92 industry standards for guaranteed bitrates (GBR) to ensure quality of service for voice traffic.

“As cellular networks grow increasingly congested, operators are constantly striving to find ways to manage traffic,” said Heikki Tenhunen, senior vice president of Renesas Mobile Corporation. “By being able to manage many more services in all-IP networks, operators are able to free the spectrum used for legacy circuit switched GSM and WCDMA networks. This demonstration shows that Renesas Mobile is helping operators move in this direction.”

For VoLTE, the voice call utilizes the IP Multimedia Subsystem (IMS) that has already been deployed by many operators on LTE networks. VoLTE not only optimises network efficiency and enables higher quality voice and messaging over IP, it also provides the foundations for a broad range of services such as real-time video and various rich media and collaboration services that can interact with Web applications, potentially generating major new revenue streams in consumer and enterprise markets.

The VoLTE capability will be available across a wide range of our product portfolio of slim modems and communications processor based platforms.

About Renesas Mobile Corporation

Renesas Mobile Corporation (RMC) is a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723) and offers advanced and innovative products and services for mobile phones, car infotainment solutions, consumer electronics and industrial applications. Renesas Mobile's mission is to develop, productize and deliver communications centric semiconductor chipsets and complete hardware and software platforms built on these chipsets to meet the needs of our customers in these markets. Renesas Mobile provides complete cellular chipset platform solutions including powerful applications processors, leadership and industry reference cellular modems, highly integrated radio frequency devices and intelligent power management solutions. Renesas Mobile offers our customer complete system and software expertise to develop flagship devices more rapidly.

(Remarks)
“Android” is a trademark of Google Inc. Other names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする