1. Home
    2. Press Center
    3. 2018
Stock Price
Investor Relations

Renesas Electronics Ships New RV2X6376A Series of 25 Gbps Directly Modulated Laser Diodes for 4.9G and 5G LTE Base Stations

Enables High-Speed Optical Communications and Stable Operation in Harsh Environments up to 95°C for Next-Generation Mobile and IoT Networks

TOKYO, Japan, March 13, 2018 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the RV2X6376A Series of directly modulated laser (DML) diodes. The DML diodes deliver 25 Gbps x four wavelengths as the light source in 100 Gbps optical transceivers that enable high-speed communications inside 4.9G and 5G LTE base stations, and between data center routers and servers. The RV2X6376A Series are the industry’s first DML diodes that support full 25 Gbps speed (per individual laser) and industrial temperature (-40°C to 95°C) without cooling.


The RV2X6376A Series are designed into compact 100 Gbps QSFP28 optical transceiver modules that use conventional NRZ modulation. They are compatible with the Coarse Wavelength Division Multiplexing (CWDM4) standard that specifies four lanes of 25 Gbps optically multiplexed onto and demultiplexed from duplex single mode fiber. The RV2X6376A Series extend the laser diodes family, joining the proven, commercial temperature grade (-5°C to 75°C) NX6375AA Series used in data centers. In addition to providing the ruggedness and reliability base stations require, the RV2X6376A Series also offers data center customers an upgrade to the wider industrial temperature range when additional margin is needed.


Mobile communications and the Internet of Things (IoT) are driving high-speed optical communication systems, which are experiencing rapid growth due to an explosion of data usage. The Cisco® Visual Networking Index (VNI) forecasts global mobile data traffic to grow 44 percent annually from 11,000 Petabytes/month in 2017 to 48,000 Petabytes/month in 2021. To service this hyper-growth, base station manufacturers are transitioning to interim 4.9G and higher throughput, low-latency 5G technology.

“The RV2X6376A Series offers manufacturers the highest reliability solution for rugged outdoor 4.9G and 5G base station applications,” said Diwakar Vishakhadatta, Vice President for High-Speed Optical Communications and Wireless Products at Renesas Electronics Corporation. “The bare die diodes’ wide temperature range and DML technology allow transceiver designers to achieve significantly lower systems cost than current designs using EML diodes.”


Key Features of the RV2X6376A Series

  • 1.3um AlGaInAs Direct Modulated DFB laser diode
  • Uncooled operation (absolute maximum ratings): Tc=-40℃ - +95℃
  • Output power: Po=7mW @ 25℃
  • SMSR: 35dB min
  • Laser operating current: 55mA max
  • Laser reverse voltage: 2.6 V max
  • High Reliability: MTTF of 100,000 hours (Note: MTTF not guaranteed)



Samples of the bare die RV2X6376A 25 Gbps laser diodes are available now and mass production starts today. For more information, please visit www.renesas.com/ products/optoelectronics/fiberoptic-devices/lasers-ofc.html. (Availability is subject to change without notice.)


Part NumberChannel NumberPeak Emission Wavelength
RV2X6376ACCWT-AAY270Channel 01270nm Lane
RV2X6376ACCWT-AAY290Channel 11290nm Lane
RV2X6376ACCWT-AAY310Channel 21310nm Lane
RV2X6376ACCWT-AAY330Channel 31330nm Lane

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live—securely and safely. A global leader in microcontrollers, analog, power and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics, Office Automation and Information Communication Technology applications to help shape a limitless future. Learn more at renesas.com.

(Remarks) Cisco is a registered trademark of Cisco and/or its affiliates in the U.S. and other countries. All registered trademarks or trademarks are the property of their respective owners.

The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.