Low Voltage Motor Control with Enhanced Operation

Low Voltage Motor Control with Enhanced Operation

Reducing power consumption, physical size, and design costs are key challenges in the consumer appliance industry. Renesas offers a wide range of MCUs tailored for motor drive applications.

RZ/V Defect Detection in the Industrial Field

RZ/V Defect Detection in the Industrial Field

This article uses PCB defect detection as an example to introduce the structure of the YOLOv3-tiny defect detection AI algorithm, the deployment process, and inference performance in Renesas RZ MPUs.

RX26T new lineup expansion : Suitable for Motor Control Applications

RX26T New Lineup Expansion: Suitable for Motor Control Applications

We've released the RX26T (RAM48KB) product as a new addition to the RX26T group lineup. For those seeking a higher-performance and more advanced microcontroller for motor/inverter control, it is go-to choice.

Renesas Powers a New Space Race

Renesas Powers a New Space Race

This blog discusses Renesas’ high-reliability (Hi-Rel) business, what’s driving the space race for Renesas, and what lies ahead.

Experience Digital Signal Processing  with RX MCU on the Cloud!

Experience Digital Signal Processing with RX MCU on the Cloud!

This blog introduces the RX Family DSP Solution on Lab on the Cloud, where you can connect to the RX microcontroller's evaluation board online and experience DSP firsthand

<style type="text/css">@media (min-width: 996px) { .col-lg-7.first_blog_p { padding-left: 50px; }} @media (max-width: 995px) { .col-lg-7.first_blog_p { padding-top: 50px; }} </style> <div class="row"> <div class="col-lg-5" style="padding: 20px 20px 0px 20px;border: 1px solid #e1e0e0; border-radius: 4px;"> <h4>Radar Transceivers: Key Components for ADAS &amp; Autonomous Driving</h4>  <ul> 	<li><a data-entity-substitution="canonical" data-entity-type="node" data-entity-uuid="d18059ba-52f0-4c58-9978-db1070c9bd

How to connect the antennas?

At mmWaves the interfaces between the radar MMIC and the antennas need to be carefully designed to avoid any degradation on the system performance. This issue of the blog will highlight some aspects that need to be considered in the design of the transitions for different antenna configurations.

Configuration Issues with the RA6 Ethernet Controller

Configuration Issues with the RA6 Ethernet Controller

Are you having issues with the Ethernet controller on the RA6 MCU family? This blog suggests that you should check the configuration of the Arm® TrustZone® boundaries and explains why.

Let's Make a Game Using a Microcontroller Blog - Part 2

Let's Make a Game Using a Microcontroller - Part 2

This blog introduces the components and circuit diagram used in the hardware design to build a falling block puzzle game with an RL78 microcontroller. The source code is also available.

Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

The Renesas RZ/G2M platform is the first RZ/MPU platform to be officially certified by Arm as compliant with SystemReady IR 1.1, a set of interoperability specifications targeting edge and IoT devices.

Single MCU Solution for Safety-Related Applications Using TrustZone Blog

Single MCU Solution for Safety-Related Applications Using TrustZone

Learn how RA 32-bit MCUs enable implementing a Class C application on a single microcontroller.