160MHz Wi-Fi Clients - It's Not All About Throughput!
Wi-Fi 6, the next generation of wireless technology, offers higher speeds and improves signal reliability, network capacity and efficiency in dense deployments.
Wi-Fi 6, the next generation of wireless technology, offers higher speeds and improves signal reliability, network capacity and efficiency in dense deployments.
The RX671 microcontroller with enhanced computing capabilities and function has contributed to the evolution of smart home appliances and industrial equipment.
To solve recent factory automation issues, Renesas proposes an RX72M Motor + EtherCAT single-chip solution, which realizes application processing, standard EtherCAT communication and motor control.
This blog provides an overview of the Ka Satcom band LNA lab demo that achieved a new performance benchmark for active beamforming ICs in electronically steered phased array antennas with two simultaneous beams.
Renesas’ Lab on the Cloud bridges the gap between ordering evaluation boards and testing in the lab by providing access to live boards in a physical lab through an online interface.
In this blog, we describe a proof of concept (POC) where we compare the benefit of having two virtual machines (VMs) sharing an integrated hardware switch against a software switch.
This blog details the benefits of the Verified Linux Package which incorporates an industrial-grade Linux Civil Infrastructure Platform Super Long-term Support kernel in the RZ/G series’ Board Support Package.
Using two of our already commercially available motor evaluation kits, users can control dual motors simultaneously by changing the motor control parameters on the simple provided GUI.
Easily get actual wireless and power evaluation even at a very early stage of the development using the Silex wireless evaluation board and Renesas’ IDE.