Monitor Program for M32C/80, M16C/80 and M16C/60 Series. After the Monitor Program is written to the MCU and the Monitor Program communicates with the Debugger, the user program can be debugged.
|
|
|
---|---|---|
Type | Title | Date |
Manual - Development Tools | PDF 1.23 MB 日本語 | |
Manual - Development Tools | PDF 1.23 MB 日本語 | |
Release Note | PDF 202 KB 日本語 | |
Release Note | PDF 172 KB 日本語 | |
4 items
|
* You can download the Monitor Programs and the Debuggers from the "Documentation & Downloads".
The operating environment depends on your debugger.
M16C R8C FoUSB/UART debugger (High-performance Embedded Workshop Version),
M32C FoUSB/UART debugger (High-performance Embedded Workshop Version)
Item | Description |
---|---|
PC | IBM PC/AT or compatible PC with Intel Pentium III 600MHz or higher |
OS | Windows XP, Windows 2000, Windows ME, Windows 98 SE (98) |
Memory | 128MB or higher |
Interface | 9-pin D-SUB Serial Interface |
M16C R8C FoUSB/UART debugger (KD30 Version),
M32C UART debugger (KD308 Version),
M32C FoUSB/UART debugger (KD3083 Version)
Item | Description |
---|---|
PC | IBM PC/AT or compatible PC with Intel DX4 100MHz/Pentium II 75MHz or higher |
OS | Windows XP, Windows 2000, Windows ME, Windows 98 SE (98), Windows 95 |
Memory | 16MB or higher |
Interface | 9-pin D-SUB Serial Interface |
The serial port of MCU is used for communication between the monitor program and debugger.
The serial port used by the monitor program is shown below.
MCU | Channel | RxD (Reception) | TxD (Transmission)* | |
---|---|---|---|---|
M16C/62A, 62M | 1 | P6_6/RxD1 | P6_7/TxD1 | * Please connect a pull-up resistor (approx. 5kΩ) to the TxD pin. |
M16C/80 | 1 | P6_6/RxD1 | P6_7/TxD1 | |
M32C/83 | 1 | P6_6/RxD1 | P6_7/TxD1 |
The monitor program offered by Renesas uses the same serial port as the flash programmer supporting Renesas Standard Serial I/O Mode 2 (serial programming mode). Therefore, if the circuit for reference use of the flash programmer which supports Standard Serial I/O Mode 2 is used, you can easily create the environment from writing the monitor program to MCU to debugging.
Renesas provides M16C Flash Starter as a flash programmer supporting Standard Serial I/O Mode 2.
Example: M30624FGA (ROM:256KB, RAM:20KB)
Example: M30800FC (ROM:128KB, RAM:10KB)
Example: M30833FJ (ROM:512KB, RAM:31KB)
<<KD debugger does not have a plan to revise any more.>>
* Target product : M32C M16C UART Monitor Program | R8C UART Monitor Program
[Latest Version]
[How to upgrade to the latest version]
Download free updates from the "Documentation & Downloads". Upgradable from any previous versions.
[How to install]
Each emulator and monitor debugger is not bundled with High-performance Embedded Workshop. Please download from the "Documentation & Downloads" on this page. Installing this emulator debugger add High-performance Embedded Workshop environment a debugging function.
[Latest Version]
Released Date | Software name | Version |
---|---|---|
9. June, 2004 | KD30 (M16C R8C FoUSB/UART Debugger) |
Ver.4.10 Release 1 |
25. August, 2004 | KD3083 (M32C FoUSB/UART Debugger) |
Ver.3.30 Release 1 |
28. May, 1999 | KD308* (M32C UART Debugger) |
Ver.1.00 Release 1 |
* KD308 is a M16C/80 Group debugger for "M32C M16C UART Monitor Program". This product has no plan to support High-performance Embedded Workshop in the future.
[How to upgrade to the latest version]
Download free updates from the "Documentation & Downloads".
The debugger depends on your MCU. In addition, the High-performance Embedded Workshop version of the debugger is the successor debugger of the KD30/KD3083 version. The High-performance Embedded Workshop version is only scheduled for release in the future.
M16C R8C FoUSB/UART debugger (High-performance Embedded Workshop Version) or
M16C R8C FoUSB/UART debugger (KD30 Version)
Family | Series | Group | Part No. | |
---|---|---|---|---|
M16C | M16C/60 | M16C/62A | M30624FGAFP/GP | M30625FGAGP |
M16C/62M | M30624FGMFP/GP | M30625FGMGP |
M32C FoUSB/UART debugger (High-performance Embedded Workshop Version) or
M32C FoUSB/UART debugger(KD3083 Version)
Family | Series | Group | Part No. | |
---|---|---|---|---|
M16C | M32C/80 | M32C/83 | M3033FJFP/GP | M30835FJGP |
M32C UART debugger(KD308 Version)
Family | Series | Group | Part No. | |
---|---|---|---|---|
M16C | M16C/80 | M16C/80 | M30800FCFP/GP | M30802FCGP |