Terminal Coplanarity

This example shows that by using the seating plane (1st datum surface S) as the standard, the vertical direction fluctuation of the bottom point of each terminal is 0.08mm or less relative to the seating plane.

See "Measuring method for Package Dimensions of BGA EIAJ ED-7304"