This webinar revolves around Wi-Fi 6 TWT, followed by DA16200's Universal-TWT feature, which is an excellent way for battery-powered devices to conserve power with no strings attached. The webinar also covers the similarities between Universal-TWT and Wi-Fi 6 TWT, as well as the advantages of Universal-TWT over Wi-Fi 6 TWT.
During this webinar we’re going to:
- Highlight the Production Line Tool - what is it?
- Show how to lower overall cost of tester equipment
- Demonstrate how easy it is to parallel program and test up to 16 devices
This webinar covers Renesas’ new RA Family entry line low-power RA2E2 MCU. This product is a new generation of microcontrollers that combine the excellent 32-bit CPU performance of Arm® Cortex®-M23 core with the Renesas superior on-chip functions and package options. Throughout the webinar, we explain why this new entry line MCU is best solution for the IoT edge devices.
Learn how to enable your process controller to communicate with Modbus devices using a modular object-based Modbus TCP stack that can serve as both master or slave (client or server) with all the function codes in a convenient portable stack.
- Provide various frameworks that will help you decide what makes sense for your next IoT product.
- Review hidden costs that you might encounter for in-house module development such as RF design resources, antenna matching, regulatory approvals, and more.
- Provide breakeven analysis templates to enable financial analysis of building in-house vs. buying from a chip vendor or a third party.
1. Introduce the DA16200 ultra-low power technology and show you how Wi-Fi can work for battery powered applications.
2. Walk through the implementation using AT-Commands (features/functions) – what it can do for your application.
3. Full end-to-end demo showing AT-Commands on the Raspberry Pi Pico board (RP2040) as a host, hooked up to the DA16200 Wi-Fi solution in an example application (Wi-Fi connected Actuator – e.g. lock or motor) all with AWS IoT services connectivity with the DA16200.
During this webinar, you will learn how the DA16200 can achieve battery lifetime measured in 'years' due to its incredible low power operation and sleep currents. We'll also demonstrate the tools and evaluation kits which can be used to achieve this great performance.
Watch this webinar to learn how Renesas' newly released 64-bit entry-level RZ/G2L and RZ/G2LC MPUs solve all the three challenges.
・High Performance CPU for New Additional Value
・System Cost Reduction
・Efficient Product Development
The Quuppa Intelligent Locating System™ is a powerful engine for various location‑based services and applications. It provides accurate real‑time positioning data using Bluetooth® Low Energy technology, unique direction finding signal processing methods, and advanced proprietary algorithms. Hosted on the amazing DA14531 BLE from Dialog (now Renesas), this out‑of‑the‑box solution provides the ultimate value in battery life, system cost, and size.
During this webinar we will:
・Highlight Quuppa Intelligent Locating System™ - What is it? How does it work?
・Show the implementation details of a DA14531‑based Quuppa positioning tag
・Demonstrate how simple it is to start prototyping using the DA14531 TINY BLE click board
Web Bluetooth® is a JavaScript API that works inside Chromium‑based web browsers. It's supported in Chrome and Edge browsers in Chrome OS, Windows 10, Android M+, Mac OS X, and Linux. Web Bluetooth takes advantage of the native Bluetooth hardware in your phone, Mac or PC, and facilitates interactions with peripheral devices directly from the browser. It brings some great advantages which can ease both development and product deployment using Bluetooth Low Energy.
During this webinar, we will cover:
・Web Bluetooth® - What Is It?
・Pros and Cons
・Examples of Web Bluetooth® and What It Can Do
・Demonstrate how simple Web Bluetooth® is to work with using our DA14531 Bluetooth® LE TINY
Dialog (now Renesas) offers the lowest power Wi-Fi SoC in the world. With our breakthrough low-power VirtualZero™ technology, IoT devices can now have a battery life of one year or more. This technology has the potential to replace existing low-power technologies such as Zigbee and Z Wave.
In this webinar, we explain:
・How the VirtualZero™-based DA16200 platform will disrupt the smart home market by simplifying the home architecture
・Why Wi-Fi will become the ubiquitous standard in smart homes
・What enables us to offer the lowest-power Wi-Fi SoC in the industry
Three industry experts will show you how to cut the cost and complexity of IoT edge‑to‑cloud connectivity, and how to introduce best practices for secure management of your IoT networks by answering these questions, and many more:
What are the risks involved in the Internet of Things?
Why, if I’m designing an IoT product, should I add the cost and complexity of security into my devices?
How do I implement seamless security throughout the supply chain – in design, production, and in the field?
Open source. Open standards. Open platforms. These keywords describe how Renesas and OpenSynergy envision the future, by investing in open technologies to make the automotive industry more flexible and independent. The Virtual I/O Device (VIRTIO™) standard and the Automotive Grade Linux (AGL) platform are open source projects accelerating the development of new features and technologies for automotive cockpit solutions. They are on the way to serve as de facto automotive industry standards.
In this free, 60-minute webinar, Thomas Bruss (Renesas) and Isaac Trefz (OpenSynergy) will deliver a unique insight into how open source projects are creating a more independent and flexible automotive industry.
Key topics & takeaways:
• Discover how Open Standards can save future mobility stakeholders time and cost
• Learn how the AGL platform can accelerate the development of new features &technologies
• Understand the impact of the VIRTIO standard on hardware and software choice
• Find out about the Renesas OSS strategy, which simplifies VIRTIO integration
• Gain insight into OpenSynergy's VIRTIO-based Hypervisor, which runs AGL on a joint reference platform with Renesas
In this webinar, we will briefly review EFTs and the issues they can cause, and then look at how Renesas' RAA78815x transceivers have the industry's highest EFT immunity and are thus the perfect solution for EFT issues.
Find out how to develop embedded products that are adaptable to design changes directly from embedded hardware subject matter of experts from Renesas and embedded GUI experts from Crank Software. Join this webinar session to learn about the latest hardware - 64-bit general-purpose RZ/G2L MPUs and PMICs (Power Management ICs)- enhancing your embedded products’ solution. Also, experience how easy it is to develop GUI apps with the Storyboard through a live demo.