Overview

Description

Topics
The following products are now supported by LLVM compiler. For details, please refer to Tool News.
[Upgrade to Revision]RL78 Family Renesas Flash Driver RL78 Type 01 SC Version V1.20 (PDF | English, 日本語)

The code flash library is free-of-charge software that reprograms the contents of the code flash memory by user programs.
"Renesas Flash Driver for RL78" is free-of-charge software that reprograms the contents of code flash memory and data flash memory by user programs.

Features

  • Flash Self Programming Libraries provide the interface for operations on the code areas of flash memories that MCUs have. (Functions are supported varies with the MCU. Please check the available functions in the user's manual for the target flash reprogramming software.) :
    • Erasing
    • Programming
    • Internal verification
    • Blank checking
    • Security settings, etc.
  • An EEPROM emulation library for code flash memory is also included.
  • Learn More

Release Information

Flash Self Programming Library Type01 for the RL78 Family

  • Latest Ver.: Ver.4.00
  • Released: Feb 05, 2024

Note: The LLVM compiler version was added to the package.

Renesas Flash Sample Program Type01 for RL78/G15 Group and RL78/G16 Group

  • Latest Ver.:  Ver.1.20
  • Released: Dec 20, 2023

Renesas Flash Driver RL78 Type 01 for RL78/G2x Group

  • Latest Ver.: Ver.1.20
  • Released: Sep 20, 2023

Renesas Flash Driver RL78 Type 02 for RL78/F23 and RL78/F24

  • Latest Ver.: Ver.1.00
  • Released: Aug 05, 2022

Details of upgrade (See Tool News)

Operating Environment

Distribution Method

Target Devices

Downloads

Documentation

Design & Development

Sample Code

Re-programming the flash memory build-in the microcomputer

This video explains how to re-program the flash memory. This focus on the mechanism of re-programming the flash memory built-in the microcomputer.

Additional Details

Distribution Method

Target Device FamilyDistribution MethodSoftware name described in the download list
V850DownloadFlash Self Programming Library  Note1
RL78/x1xDownloadFlash Self Programming Library  Note2, 3  
Renesas Flash Sample Program Type01 Note4
RL78/x2xSample CodeRenesas Flash Driver RL78 Type01 Note5  
Renesas Flash Driver RL78 Type02 Note6
78K (78K0, 78K0R)DownloadFlash self programming library  
EEPROM emulation library
RXApplication notes and sample codes for RX family related to flash programming are available. Please visit the Application Notes & Sample Code of the Documentation tab on the RX family product page.-

Notes:

  1. For the EEPROM emulation library, contact your local Renesas Electronics marketing office or distributor.
  2. In the User's Manual (Hardware) for some RL78 MCUs or the User's Manual for some Flash Libraries for the RL78 family, the self RAM areas used in common for all flash libraries may be shown. However, for the latest information, please refer to the RL78 Family Self RAM list of Flash Self Programming Library Rev.3.05 (PDF | English, 日本語).
  3. As the self RAM areas are used as the work area for the library, using these areas for the user program is prohibited. For the latest information, please refer to the RL78 Family Self RAM list of Flash Self Programming Library Rev.3.05 (PDF | English, 日本語).
  4. Renesas Flash Sample Program Type01 for RL78/G15 group and RL78 G16 group can be downloaded from Sample Code.
  5. Refer to Renesas Flash Driver and EEPROM Emulation Software for RL78 Target MCU List - General-Purpose (PDF | English, 日本語) for Renesas Flash Driver and EEPROM Emulation Software target MCUs for non automotive use.
  6. Refer to Renesas Flash Driver and EEPROM Emulation Software Target MCU List for RL78 - Automotive (PDF | English, 日本語) for Renesas Flash Driver and EEPROM Emulation Software target MCUs for automotive use.

Target Devices