Various Contracts to Satisfy Your Requirements

For real-time OS products, a software licensing agreement must be entered upon purchase of a mass-production license. However, since shrink wrap agreements are used for evaluation licenses, unsealing the product indicates your agreement to the terms of the license, and a formal software licensing agreement is not required. Agreement types and distribution are as described below.

For agreement details, contact your nearest sales office or representative.

OS Agreement Details

Agreement Type Mass-production License Evaluation License
With Source Code No Source Code No Source Code (Shrink Wrap Agreement)
Product Deliverables OS Source Code Yes No No
OS Object Code Yes Yes Yes
Sample Source Code Yes Yes Yes
Manual Yes Yes Yes
License Grant Right for Internal Use Yes Yes Yes
Right to Reproduce Yes (Unlimited) Yes (Unlimited or 3,000) (Note1) Yes (Internal use only, unlimited copies)
Right to Modify Program Yes No No
Host Machine Limitation Unlimited Unlimited Limited number of hosts (1 or Unlimited) (Note2)
Application Limitation Limited Limited Unlimited
Device Limitation Limited Limited Unlimited

Explanation of terms:
Yes: Included in the license. No: NOT included in the license.

Notes:

  1. For "right to reproduce" of the MR8C/4 mass-production license (no source code) , only "Unlimited" can be chosen.
  2. For "host machine limitation" of the MR8C/4 evaluation license, only "1" can be chosen.
Important:
License grants are valid until the Licensee informs Renesas of the relinquishment of rights. All licenses are for use only, and do not grant property rights.

Explanation of Terminology Used in the OS Agreement

Terminology Explanation
Mass-production License This license permits the Licensee to market or sell a product which incorporates the real-time OS. The mass-production license also permits prototype development. Separate purchase of an evaluation license is not necessary for development.
Evaluation License This license permits the Licensee to install the software on up to a designated number of host machines, and use in prototype development. There is no limit to the number of prototypes with built-in real-time OS which may be developed; however, the license is restricted to application in prototype development only.
Right for Internal Use The Licensee can use the real-time OS object code internally (within the Licensee's department, etc.) on supported MCUs. This right assumes that the real-time OS is used only in a prototype system for development.
Right to Reproduce The Licensee can use the real-time OS object code on multiple devices. For the mass-production license, the maximum number of reproductions must be entered in the agreement. The Licensee can choose to set the number of reproductions as either unlimited or 3000 (agreements which include source code must be unlimited). The price varies according to the number of reproductions.
Host Machine Limitation The real-time OS is provided on media such as a CD. The Evaluation License limits the number of host machines on which the contents of this media may be installed (choice between 1 or Unlimited).
Application Limitation For the mass-production license, the basic name of the Licensee's application (or project) must be written in the agreement. (For example, ink-jet printer, color copy machine for professional use, economy car navigation system, etc.) Changing to another project requires a new agreement.
Device Limitation The MCU type on which the OS is to be incorporated must be written in the agreement. A new agreement is required if the target MCU changes.

Ordering Information

Product Type Part Number
RI850V4 V2 RTRRH8500TR01w
RI850V4 V1 R0R08500TCW01w
RI600V4 R0R5RX00TCW01w
RI600PX R0R5RX00PCW01w
RI78V4 V2 RTRRL7800TR01w
RI78V4 V1 R0R07800TCW01w
RI850MP (Discontinued product) R0R085E2MCW01w
HI7000/4 R0R40700TRW02w
HI7700/4 (Discontinued product) R0R40770TRW02w
HI7750/4 (Discontinued product) R0R40775TRW02w
RI600/4 (Discontinued product) R0R5RX00TRW01w
RI600/PX (Discontinued product) R0R5RX00PRW01w
MR8C/4 (Discontinued product) R0R52100TRW01wE
M3T-MR100/4 R0R56400TRW01wE
M3T-MR308/4 (Discontinued product) R0R30800TRW02wE (Note1)
M3T-MR30/4 R0R30600TRW02wE
HI1000/4 R0R41600TXW01w

Note:

  1. M3T-MR308/4 with this part number does not support DVP-M2(S) nor DVP-C3. If you need an M3T-MR308/4 which supports DVP-M2(S) or DVP-C3, please contact your nearest Renesas Electronics sales office or distributor.
Important:
The lower-case 'w' in the part number denotes the type of license. Replace with the numeral or letter from the following table according to the type of license you want. Note that the letter to be replaced will vary depending on the real-time OS product.

Replacement Letters for the RI850V4 V2 and the RI78V4 V2

Letter Agreement Type
ERR Evaluation license, installable on one host computer.
ERRLU Evaluation license, no limit on number of host computers for installation.
RRRUL Mass-production license, allowing embedding in up to 3,000 devices, without the source code.
RRRUU Mass-production license, unlimited embedding, without the source code.
SRRUU Mass-production license, unlimited embedding, with the source code.

Replacement Letters for the Other Real-Time OS products

Letter Agreement Type
1 Evaluation license, installable on one host computer.
A Evaluation license, no limit on number of host computers for installation.
K Mass-production license, allowing embedding in up to 3,000 devices, without the source code.
U Mass-production license, unlimited embedding, without the source code.
Z Mass-production license, unlimited embedding, with the source code.
Applicable for the following Real-time OSes:
HI7750/4, HI7700/4, HI7000/4, RI850V4 V1, RI850MP, RI600V4, RI600/4, RI600PX, RI600/PX, RI78V4,MR8C/4,M3T-MR100/4, M3T-MR308/4, M3T-MR30/4, HI1000/4
Example:
In mass-production license for RI78V4 for manufacturing the unlimited number of products with the source code closed, the Part Number is R0R07800TCW01U.