1. Home
    2. Press Center
    3. 2015
Stock Price
Investor Relations

Renesas Electronics Expands Touch-Based Application Possibilities for Home Appliance, Building, and Industrial Automation Applications with RX130 Group of MCUs

New 32-Bit MCUs Bolster Lineup of High-Sensitivity Touch Key MCUs, Offering More Convenient Development Environment for Cost-Sensitive Applications

Düsseldorf, November 24, 2015 — Renesas Electronics, a premier supplier of advanced semiconductor solutions, today announced it is expanding development support for touch-based home appliance, building, industrial automation, and portable medical applications with the new RX130 Group of 32-bit microcontrollers (MCUs). The new Group allows embedded developers to incorporate both user interface (i.e., touch key) and system control capabilities in a single MCU. Developers working with capacitive touch-based applications can leverage Renesas' state-of-the-art second-generation capacitive touch technology, with self- and mutual-capacitance capability, in an ultra-low power, low-cost 32-bit MCU fabric.

 

    The new RX130 Group combines excellent sensitivity and noise tolerance, making it possible to develop touch keys employing a variety of cover materials, including thick acrylic, glass, wood, fabric, or stone, for use in a broad array of new applications. These include control panels for electric appliances used in locations where they are likely to get wet, home equipment employing recessed switches for a more attractive design, and industrial machinery that must be operated with gloves on for safety reasons.

 

    The new RX130 Group complements the existing lineup of Renesas MCUs supporting capacitive touch-based applications, including: the RX231 Group for high-end electric home appliances and industrial machinery, supporting DSP/FPU (Note 2) and enhanced security and communication functions; and the RX113 Group for home equipment and healthcare devices, with LCD display and USB communication functions. With the addition of the new RX130 Group, Renesas' lineup of touch key MCUs comprises 256 product versions in total, with flash memory capacities ranging from 64 KB to 512 KB and number of pins ranging from 48- to 100-pins. Pin compatibility and software compatibility are maintained between the RX231 and RX130, making it possible to reuse existing software resources and providing coverage for devices from mid- to low-end to high end.

 

 

Key features of the RX130 Group:

  • (1) Ability to detect up to 64 touch keys for simplified board design

    The RX130 MCUs can support complex user interface requirements with support for up to 36 touch keys in self-capacitance mode and up to 36 keys through matrix configuration. The RX130 Group also offers mutual capacitance mode, which allows the number of touch keys to be expanded up to 64, among the most supported anywhere. This reduces the wiring complexity when adding a touch panel and helps simplify the board design. The high-speed processing of the 32-bit CPU means that the load on the CPU is less than 10 percent even during 64-key control. The RX130 Group allow the developer to run very processor intensive applications, while still managing the capacitive touch interface.

 

  • (2) Industrial-leading low touch key standby current among the lowest in the world for reduced power load

    Using an on-chip oscillator operating at 15 kHz (kilohertz), a low-power timer that consumes very little power wakes the CPU from the idle state at regular intervals to detect contact with the touch panel. This enables the RX130 Group to achieve an industrial-leading low standby current of approximately 8μA (Note 1). The low standby current helps reduce the power consumption load imposed when adding a touch key, which enables capacitive touch capabilities for battery-operated and other portable devices with low power consumption requirements.

 

  • (3) Improved support for touch key adoption thanks to expanded selection of reference software and documentation needed for development

    Using the Workbench6 automatic calibration tool with Renesas touch key MCUs makes it possible to use a graphical user interface (GUI) to adjust the sensitivity and other settings easily, something that was previously complicated by the effects of factors such as the board layout and tracing pattern, the panel material, etc. Future upgrades to Workbench6 will allow it to be used not only as a development tool but, in conjunction with software and information needed for development that is also being made available, including application notes, user's manuals, and reference software, it will be possible to use Workbench6 with a sample MCU and an evaluation board to confirm and evaluate system operation immediately. An RX130 touch-based evaluation kit that includes Workbench6 is scheduled to be available in February 2016.

 

 

Availability

Samples of the RX130 Group are available now. Mass production is scheduled to start in March 2016.

Refer to the separate sheet for main specifications of the RX130 Group.

 

(Note 1) Standby current for one touch panel channel with a period of 100 ms.

 

(Note 2) Digital signal processor/floating point unit

 

(Note 3) An integrated development environment supporting Renesas RX family MCUs (RX600, RX200, and RX100) that is based on Eclipse, an open source integrated development environment in widespread use worldwide, and CDT plugins that allow use of the C/C++ language for development.

 

 

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at at www.renesas.com.
Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.

 

Remarks
All registered trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Contact