Cyberon CSpotter

Renesas RA Family Partner Solutions
Added on 2019-12-13

Cyberon CSpotter is a local voice trigger & command recognition solution that consumes very low resources and provides high-accuracy performance running on RA with 120Mhz speed to support multi-languages as well as H/W crypto engine for security.



Related Videos

2:15
Introducing Renesas' RA ready software and hardware building block solutions for the IoT.
1:19
The Cypherbridge uLoadXL secure boot and safe software update software solution is integrated with the RA FSP and the SDKPac toolkit for RA Family devices.
1:29
The Cypherbridge SDKPac secures IoT applications such as this light sensor using the Silex Wi-Fi Pmod to connect to the Microsoft Azure cloud on the RA6 evaluation kit.
6:29
The Veridify DOME™ solution delivers a flexible onboarding and ownership management blockchain platform for low-resource IoT edge devices like RA6 MCU series.
3:15
The GT&T Fleet and Asset Tracker is a small and reliable GPS fleet tracker based on the Renesas RA6M3 processor family.
1:49
The FSP software for the Renesas RA family includes SEGGER emWin, an embedded GUI solution for creating efficient and high-quality GUIs.
3:15
Cyberon CSpotter is a local voice trigger & command recognition solution that uses low resources and provides high-accuracy performance on Renesas RA MCUs.
1:51
With the CapExt capacitive touch simulation tool, you can ensure optimal touch performance before the first prototype.
2:02
Renesas provides a voice recognition solution with low clock and small memory size compared to conventional products, without the need for an internet connection.
15:47
Get an overview of Multizone and watch a live demo of it running three equally secure zones on the RA EK-RA6M3 development board.
2:15
Introducing Renesas' RA ready software and hardware building block solutions for the IoT.
1:19
The Cypherbridge uLoadXL secure boot and safe software update software solution is integrated with the RA FSP and the SDKPac toolkit for RA Family devices.
1:29
The Cypherbridge SDKPac secures IoT applications such as this light sensor using the Silex Wi-Fi Pmod to connect to the Microsoft Azure cloud on the RA6 evaluation kit.
6:29
The Veridify DOME™ solution delivers a flexible onboarding and ownership management blockchain platform for low-resource IoT edge devices like RA6 MCU series.
3:15
The GT&T Fleet and Asset Tracker is a small and reliable GPS fleet tracker based on the Renesas RA6M3 processor family.
1:49
The FSP software for the Renesas RA family includes SEGGER emWin, an embedded GUI solution for creating efficient and high-quality GUIs.
3:15
Cyberon CSpotter is a local voice trigger & command recognition solution that uses low resources and provides high-accuracy performance on Renesas RA MCUs.
1:51
With the CapExt capacitive touch simulation tool, you can ensure optimal touch performance before the first prototype.
2:02
Renesas provides a voice recognition solution with low clock and small memory size compared to conventional products, without the need for an internet connection.
15:47
Get an overview of Multizone and watch a live demo of it running three equally secure zones on the RA EK-RA6M3 development board.
2:15
Introducing Renesas' RA ready software and hardware building block solutions for the IoT.
1:19
The Cypherbridge uLoadXL secure boot and safe software update software solution is integrated with the RA FSP and the SDKPac toolkit for RA Family devices.
1:29
The Cypherbridge SDKPac secures IoT applications such as this light sensor using the Silex Wi-Fi Pmod to connect to the Microsoft Azure cloud on the RA6 evaluation kit.
6:29
The Veridify DOME™ solution delivers a flexible onboarding and ownership management blockchain platform for low-resource IoT edge devices like RA6 MCU series.
3:15
The GT&T Fleet and Asset Tracker is a small and reliable GPS fleet tracker based on the Renesas RA6M3 processor family.
1:49
The FSP software for the Renesas RA family includes SEGGER emWin, an embedded GUI solution for creating efficient and high-quality GUIs.
3:15
Cyberon CSpotter is a local voice trigger & command recognition solution that uses low resources and provides high-accuracy performance on Renesas RA MCUs.
1:51
With the CapExt capacitive touch simulation tool, you can ensure optimal touch performance before the first prototype.
2:02
Renesas provides a voice recognition solution with low clock and small memory size compared to conventional products, without the need for an internet connection.
15:47
Get an overview of Multizone and watch a live demo of it running three equally secure zones on the RA EK-RA6M3 development board.