How to set up and use TraceX® in a Renesas Synergy™ project using IAR Embedded Workbench

Added on 2018-06-27

Getting a detailed view of the behavior of embedded application software becomes crucial not just for debugging but also for performance optimization.

Related Videos



Video Transcript

Optional Transcript goes here if available. Read through the transcript text and link any appropriate keywords and products that have pages.

Example:

There are many 12V rails in industrial applications today that need a buck converter to step the voltage down to a lower voltage and deliver up to 14 amps. The ISL85009, ISL85012 and ISL85014 are pin compatible, very efficient and are able to deliver up to 14 amps.