A Tiny RX23E-A Board for Digital Load Cell
The RX23E-A, which integrates an MCU and high-precision Analog Front End on a single chip, is ideal for realizing integrated sensing and signal conditioning of a digital load cell in the same housing.
The RX23E-A, which integrates an MCU and high-precision Analog Front End on a single chip, is ideal for realizing integrated sensing and signal conditioning of a digital load cell in the same housing.
With an ASIC solution, all the condition monitoring circuitry can be placed on the same chip with all the required electronics for the core function of the product.
In this blog, we give a brief background summary of PCIe, what its potential PCIe use cases are and what needs to be looked at to smoothen the adaption path of PCIe in future automotive applications.
The RX family of 32-bit MCUs offers evaluation kits with Azure Certified Device certification, sample code and IDE for deploying Azure RTOS. These enable easy connection to Azure IoT Hub.
H8SをFPGAに組み込んだ実装例を元にFPGAマイコンをご紹介します。
This blog introduces the xEV market status in Europe, one of the most active areas, and our promotional activities.
This blog introduces our turnkey solutions for smart cameras collaborating with LUPA in order to achieve a very short time to market.
This solution demonstrates a single motor technique (120-degree/trapezoidal) for BLDC motor control using the Renesas RX13T 32-bit MCU for motor control.
In this blog, we explain the trend of deep learning architecture in the next generation of autonomous driving cars.
This blog presents the benefits of Renesas’ Remote Industrial Process Monitoring System Solution.