EV用充電ステーションの市場動向と技術トレンド
現在、世界中で自動車の電動化(EV化)が急速に進んでいます。一方で、EVが普及するためには、充電ステーションの普及が重要です。本ブログでは、EV用充電ステーションの市場動向と技術トレンドを紹介します。
現在、世界中で自動車の電動化(EV化)が急速に進んでいます。一方で、EVが普及するためには、充電ステーションの普及が重要です。本ブログでは、EV用充電ステーションの市場動向と技術トレンドを紹介します。
This series of blogs (in three parts) discusses how noise can affect a microcontroller system and provides design ideas on how a microcontroller system can be made more robust in the presence of noise.
Renesas offers a comprehensive AC Servo Kit solution, using the RZ/T2L MPU and features servo control with various communication protocols, as well as field sensors for data collection via remote IO.
This blog looks at how we can correct soft errors in the RA microcontroller family SRAM it discusses how soft errors occur, and looks at how our implementation of an error correction function in the SRAM can both detect and correct these errors.
AC-DC電源制御の例としてRXマイコンによるトーテムポールインターリーブPFCの制御方法を紹介します。
This series of blogs (in three parts) discusses how noise can affect a microcontroller system and provides design ideas on how a microcontroller system can be made more robust in the presence of noise.
Recently MPUs have many functions and the setting of shared pins that assign multiple functions to one pin has become complicated. In addition, the number of pins has increased. So, it became difficult to set pin configurations manually without making mistakes. In this blog, “Smart Configurator for RZ” is introduced for Linux on RZ MPU series.
2モータ+PFC制御を1チップで実現できる新RXマイコン RX26Tをご紹介します。
This series of blogs (in three parts) discusses how noise can affect a microcontroller system and provides design ideas on how a microcontroller system can be made more robust in the presence of noise.
全てのRXファミリマイコンでSPI接続のTFT LCDモジュールを制御できるソリューションです。洗練されたHMIを少ないハードウェアリソースで実現できます。