What is data acquisition (DAQ) and distributed processing/edge computing in the IoT era with RX23E-A?

RX23E-AによるIoT時代のデータアクイジション(DAQ)と分散処理/エッジコンピューティングとは?

高精度AFE内蔵マイコンRX23E-Aと産業ネットワーク機能を強化したマイコンRX72Mを組み合わせることで、IoT時代にマッチしたデータアクイジション(DAQ)を実現することが可能です。

Dataline performance of two new actors in the networking arena

The Art of Networking (Series 4): CAN XL and 10BASE-T1S – Dataline Performance of Two New Actors in the Networking Arena

This blog gives a brief overview of CAN XL and 10MBit/s Ethernet, and the differences between them.

Functional Safety over EtherCAT Blog

ルネサスによる、Functional Safety over EtherCATへの取り組み

ルネサスが2020年後半にFSoEソリューションを発売して以来、このソリューションは世界中から注目されています。このブログでは、ルネサスのFSoEソリューションがどのように開発を容易にし、且つ開発期間を短縮するのかをご紹介します。

Healthy Air in Schools and Public Buildings Blog

Healthy Air in Schools and Public Buildings

The Renesas RTD120D two-channel silicon-based thermopile can support healthy air in Canadian classrooms.

Obtain the Latest Information at the “Virtual Renesas Automotive Days”!

「Renesas Automotive Days オンライン」で最新情報をご入手ください!

“ルネサスの戦略と幅広い車載ソリューションラインナップをアップデートさせていただく機会として「Renesas Automotive Daysオンライン」を開催します。

160MHz Wi-Fi Clients - It's Not All About Throughput!

160MHz Wi-Fi Clients - It's Not All About Throughput!

Wi-Fi 6, the next generation of wireless technology, offers higher speeds and improves signal reliability, network capacity and efficiency in dense deployments.

The RX671 Microcontroller Meets the Ever-evolving Demands of IoT Devices Blog

進化し続けるIoT機器の要求にお応えする新製品RX671

家電や産業機器の進化・IoT化に貢献してきたRX600シリーズに新製品RX671が加わりました。演算能力・機能が強化されたRX671の追加で、より幅広いニーズへの対応が可能となりました。

RX72M Single-Chip Motor Control via EtherCAT Communications

RX72M EtherCAT 通信を用いたシングルチップソリューション

ルネサスはアプリケーション処理と標準的なEtherCAT通信、モータ制御をワンチップで実現するRX72M モータ+EtherCAT シングルチップソリューションをご提案します。

Ka-band Rx Beamforming IC Blog

Successful Demonstration of Next-Gen Ka-band Rx Beamforming IC Portfolio with 1.5dB NF LNA

This blog provides an overview of the Ka Satcom band LNA lab demo that achieved a new performance benchmark for active beamforming ICs in electronically steered phased array antennas with two simultaneous beams.

Accelerate Your Design Process with Renesas’ Lab on the Cloud

Accelerate Your Design Process with Renesas’ Lab on the Cloud

Renesas’ Lab on the Cloud bridges the gap between ordering evaluation boards and testing in the lab by providing access to live boards in a physical lab through an online interface.