The July update of Renesas 365 builds on its System Data Model foundation with enhancements across system design, device configuration, and platform performance.
Developers can now move more efficiently between system, hardware, and software workflows when creating and refining Renesas-based MCU solutions.
Visual Studio Code Integration for Renesas 365
Renesas 365 is now integrated with Visual Studio Code, enabling the development of Renesas C/C++ projects for the RA device family.
This integration brings the same Renesas 365 capabilities available in Renesas e2 studio to Visual Studio Code. Developers can access system-aware configuration, connected workflows, and cross-domain capabilities while working in their preferred environment without sacrificing functionality.
For information on using the Renesas VS Code extension, visit here.
Automatic Synchronization of Functional Block Ports and Peripheral Instances
Functional block ports are now automatically synchronized with device model peripheral instances when a Renesas 365 solution is created from an existing e2 studio software project or a ready-to-run example.
As part of solution creation, Renesas 365 performs an automatic Engineering Change Order (ECO) to populate and align the Electronic System Designer (ESD) document with the imported system model.
The result is a smoother onboarding experience for imported and preconfigured designs, reducing setup effort while keeping developers in control of subsequent changes.
Electronic System Designer Web Editor Improvements
Renesas 365 introduces several usability improvements to the Electronic System Designer (ESD) web editor, with a focus on reducing manual effort and making system designs easier to create and maintain.
ESD now automatically expands hardware blankets when associated functional blocks change, helping maintain alignment as designs evolve.
In addition, functional blocks and other ESD objects can now be rotated, which provides greater flexibility when organizing diagrams while preserving existing connections.
Additional enhancements include automatic parameter updates during copy and paste operations, and faster editing of functional blocks and their associated objects.
Expanded Symbol Library with AC Power Support
Electronic System Designer now includes AC power symbols as part of its available symbol library.
These symbols integrate alongside existing components and functional blocks, allowing power elements to be defined and connected within the same system-level design environment.
This addition helps developers create more complete system representations and makes it easier to bring real-world designs into Renesas 365.
Improved Device Configuration and Change Visibility
Renesas 365 introduces several enhancements to the Device Configuration experience, improving how changes are reviewed and applied.
Peripheral instances can now be selected directly within the comparison interface, with corresponding pins highlighted in the device visualization. This provides a clearer connection between configuration changes and their physical implementation.
Additional flexibility has also been introduced for working with virtualized peripherals. Device configuration now supports the removal of ports, allowing developers to directly manage configurations in scenarios such as ADC setup.
New In-App Help and Learning Experience
Renesas 365 now includes a dedicated in-app help experience, providing direct access to learning and support resources within the platform.
Developers can explore video content and recent feature updates, access documentation articles, and find answers to common questions in the same space.
Reference Design and Evaluation Kit Enhancements
We’ve expanded support for reference design and evaluation workflows with broader device compatibility and updated software integration.
This includes support for additional Renesas RA Wireless modules such as the RA6W1, RA6W2, and RRQ61xxx families, along with integration of Renesas Flexible Software Package (FSP) version 6.4.0.
DEBUG peripheral configuration is also now supported across the full device portfolio, improving consistency when working with development and evaluation setups.
Platform Performance Improvements
Significant performance and efficiency improvements have been made across device modeling and the WebIDE experience.
A new constraint resolver engine delivers faster device configuration generation while significantly reducing memory usage. Additional enhancements improve support for more complex configurations, helping make device modeling and configuration more responsive.
WebIDE performance has also been improved, reducing the time required to open software projects, inspect source files, and navigate from software-defined pins directly to their corresponding locations on the PCB.
Together, these improvements help developers move more quickly between configuration, software review, and implementation activities.
Improving Everyday Development Workflows
Together, these updates strengthen key areas of the Renesas 365 experience, from system design and device configuration to platform performance. They help developers create solutions more efficiently, better understand design changes, and move more quickly from evaluation and configuration to implementation.