RX100 series: the industry’s lowest cost, ultra-low power 32-bit RX devices achieve as little as 350nA current consumption

2013年2月25日

Dusseldorf, February 25, 2013 – Renesas Electronics Europe, a premier provider of advanced semiconductor solutions, today disclosed details of its roadmap for its next-generation microcontrollers (MCUs). Renesas is expanding the RX family to include the lowest power, lowest cost RX 32-bit MCU for the embedded market, integrating as little as 8KB of flash memory.

The RX Family

The RX family from Renesas now includes devices from 8KB to 8 MB of embedded flash memory with compatible instruction set, peripherals and hardware and software tools set. The Renesas RX family has been designed to support a wide range of applications, from small MCU application equipment for which cost is the most important factor, to applications that require high data processing performance.

The high end of the RX family, the RX600 series based on 90nm technology, incorporates the industry’s fastest embedded flash memory based on Renesas’ MONOS technology, enabling single cycle access as high as 100MHz. The highest performance lineup will increase further as this family extends onto the 40nm technology node.

The low end of the RX family, the RX200 series, is the compatible solution that extends the family with devices at a lower cost and with lower power consumption. This means that designers can cover all their MCU applications with a single family using a single tool chain and re-use all their software IP across different developments.

New Low-Power RX100 Offerings

The RX100 Series MCUs, which are based on the proven 130nm, low-power process technology, can run at 32MHz, delivering 1.56DMIPS/MHz throughput, consuming only 110uA/MHz power in full active mode and targeting only 350nA in the standby mode. This achieves an even lower cost and power consumption than the RX200 series already in the market. With this new series, the RX family provides a platform with a common core, using common tools and common peripherals.

The RX100 series is clearly targeting low power applications such as wearable / battery powered applications including medical and sensor products. Due to the low system cost of the RX100 series, Renesas will also be able to compete very effectively in the ultra-low end market space where cost is the most important decision factor.

The very impressive figure of only 350nA current consumption and 70uA/DMIPS is the kind of power consumption typically only found in the 8-bit market. With this new series, customers have the option of using a 32-bit microcontroller where they previously had no choice but to use an 8-bit MCU.

Availability

The first samples of the new RX100 product series, the industry’s lowest cost, ultra-low power 32-bit RX devices offering flash memory integration from 8KB to 128KB, are now available and mass production is scheduled for 4Q of 2013.

(Remarks)
All product names and service names that appear in this press release are all trademarks or registered trademarks of their respective owners.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする