2013年11月28日

Dusseldorf, November 28, 2013 — Renesas Electronics Europe, a premier provider of advanced semiconductor solutions, has teamed up with its alliance partner Technologie Management Gruppe (TMG) to offer comprehensive software support for its multi-protocol industrial Ethernet solutions. TMG is implementing PROFINET and EtherNet/IP stacks from Molex on the Renesas Industrial Network (R-IN) devices, providing customers with easy access to these technologies and a fast market entry.

With its revolutionary hardware accelerator design, Renesas' R-IN32M3 multi-protocol industrial Ethernet solutions are 5 times more efficient in Ethernet packet processing, while reducing overall power consumption by 50%. EtherCAT and CC-Link IE real-time protocols are implemented in hardware, offering the most robust implementation while limiting the impact on the overall power dissipation. Software based protocols like EtherNet/IP, PROFINET RT, and Modbus TCP run on the ARM® Cortex M3 processor with 1.3MB embedded RAM attached. Due to the high degree of integration, the R-IN devices include Ethernet PHYs, various fieldbus interfaces and multiple peripheral modules.

Molex PROFINET and EtherNet/IP SDKs allow sensor, actuator and PLC manufacturers to efficiently integrate PROFINET and EtherNet/IP into their products. Molex software stack solutions provide reliable and robust performance across complex industrial networks in a wide range of advanced manufacturing and automation applications. As a technology partner of Molex, TMG has vast experience integrating Molex technologies onto a variety of devices. The availability of these internationally well respected stacks on the R-IN series of devices offers comprehensive and high quality implementations of industrial Ethernet technologies.

About TMG Technologie und Engineering GmbH

TMG TE is one of the leading service providers in industrial communication technology and focused to PROFINET, EtherNet/IP, PROFIBUS and IO-Link as well as TCI, FDT and EDD. TMG TE is member of PROFIBUS International, ODVA and the IO-Link consortium and is accredited as competence centre for PROFINET, PROFIBUS and IO-Link. TMG TE possesses own basic technology and has already realized various master and device integrations based on own or partners' technology.
Further information can be found at http://www.tmgte.de / [email protected]

About Molex Incorporated

Providing more than connectors, Molex delivers complete interconnect solutions for a number of markets including data communications, telecommunications, consumer electronics, industrial, automotive, medical, military and lighting. Established in 1938, the company operates 40 manufacturing locations in 16 countries. The Molex website is www.molex.com. Follow us at www.twitter.com/molexconnectors, watch our videos at www.youtube.com/molexconnectors , connect with us at http://www.facebook.com/molexconnectors and read our blog at www.connector.com.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com.
Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする