2014年11月5日

Dusseldorf, November 5, 2014 — Renesas Electronics Europe, a premier provider of advanced semiconductor solutions, today announced the release of the "Display it! – RX HMI Solution Kit". This is the second "Display it! – RX HMI Solution Kit" after the release of the RZ based kit on 30th October and is part of the Renesas Solution Kit initiative. This new 32-bit MCU RX based solution kit enables engineers to quickly evaluate and demonstrate the leading HMI tools in the industry, accelerating their prototyping and decision-making processes. This second "Display it! – RX HMI Solution Kit" is based on Renesas' RX63N and RX631 groups of microcontrollers.

The "Display it! – RX HMI Solution Kit" continues to drive innovation for the next generation of connected applications with HMI requirements, helping designers simplify and speed the development cycle by adding a touchscreen TFT for medical, instrumentation, home automation, energy management, fitness and transportation products.

These RX63N/RX631 groups offer up to 256kB embedded RAM and up to 2MB of embedded zero wait state Flash, and run on a 100MHz CPU clock frequency.

In terms of communication capability, the RX631/RX63N offer up to three channels of CAN 2.0B compliant interfaces, two USB full speed (Host Function/OTG Function) and device features and an Ethernet MAC IEEE 802.3 interface, compliant with MII and RMII, for easy connection to a PHY.

To cope with the HMI requirement, the RX63N/RX631 groups includes an exDMA peripheral that can transfer data over an external bus independently of the internal bus occupation. This allows these MCUs to easily support TFT solutions for up to WQVGA class TFT panels.

Based on Renesas' RX63N MCU and the 4.3-inch WQVGA graphic/touch module, the "Display it! – RX HMI Solution Kit" offers a cost-effective platform for rapid GUI development and deployment. Out of the box, the kit provides efficient testing of GUI demo software products from leading Renesas Alliance Partners, including:

  • emWIN from Segger
  • GUIX from Express Logic
  • Guiliani from TES
  • MicroEJ JVM from IS2T
  • TouchGFX from Draupner

This allows engineering teams to quickly make decisions on which software is most appropriate for their application, speeding the time to market. In addition, these boards are supported by a free of charge sample software from Renesas.

"The "Display it! – RX HMI Solution Kit" marks the next stage in our strategy of providing our customers with a tool that makes it easier for them to select the right fitting GUI software for their application needs," said Bernd Westhoff, RX Product Manager at Renesas Electronics Europe. "This is why we teamed up with our Alliance partners, including Segger, ExpressLogic, TES, IS2T and Draupner, to develop a unique GUI solution package enabling a quick and easy evaluation of these different solutions, just with one click."

Alongside the GUI demo software, the solution kit also includes the RX HMI base board with 4.3-inch WQVGA graphic/touch display, compiler, debugger and IDE – everything engineers need to start their HMI development once they have selected the HMI software they require.

The "Display it! – RX HMI solution kit" is part of a range of next generation solution kits that Renesas will be launching at electronica 2014 in November (Hall A6, Stand 243). It will be available for ordering via Renesas' franchised distribution partners after the event. The solution kit's part name is YDISPLAY-IT-RX. Additional technical details are available at www.renesas/rxhmi.

(Remarks)
All product names and service names that appear in this press release are all trademarks or registered trademarks of their respective owners.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする