Visit Booth #608 for Demonstrations on Industrial, Power Supply, Lighting, and HVAC

2013年3月18日

SANTA CLARA, Calif., March 18, 2013 — Renesas Electronics America Inc., a premier provider of advanced semiconductor solutions, will showcase several of its power technologies at the Applied Power Electronics Conference (APEC), March 17-21, taking place at the Long Beach Convention Center in Long Beach, Calif. Demonstrations in booth #608 will highlight the company's power solutions portfolio designed to enable a Smart Society. These include microcontroller (MCU)-based solutions optimized for applications such as industrial, power supply, lighting, and home appliances.

Renesas Product and Technology Demonstrations

Scalable 3 Phase AC Motor Drive Platform:

This interactive demo will showcase a complete, scalable, AC/BLDC motor drive hardware + software evaluation platform with a front end dual interleaved AC-DC PFC stage, and a 3 phase inverter bridge, implemented by high efficiency IGBTs and FRDs. A high performance 32-bit MCU (RX62T) enables implementation of algorithms for high efficiency motor drives in applications such as air-conditioners, and industrial motor drives by providing a complete proven system solution.

Thin Wafer IGBT with 70µm Thickness:

The newest IGBTs from Renesas will be on display. These are based on the enhanced Thin Wafer trench HiGT (High conductivity IGBT) technology enabling high efficiency solutions in industrial applications such as motor drives and solar inverters.

120V to 24V AC: AC Converter:

This new hardware IP achieves twice the encoding/decoding performance of the earlier Renesas products, namely full HD video at 60 fps (1080p60), with the same hardware scale and power consumption as the earlier hardware IP. Applications that require simultaneous encoding/decoding of multiple video streams, such as compressed transcoding or video chat, can be easily implemented with a single hardware IP.

Renesas will also be showcasing its innovative optical image stabilization solution and its award-winning near field communication (NFC) charger.

About Renesas Electronics America Inc.

Renesas Electronics America Inc., headquartered in Santa Clara, California, is a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), the world's number one supplier of microcontrollers and a premier supplier of advanced semiconductor solutions including microcontrollers, SoC solutions, and a broad range of analog and power devices. In the Americas, Renesas Electronics America markets and sells industrial-type active-matrix LCD modules from NEC LCD Technologies, Ltd., a global leader in innovative display technologies. More information about the products offered by Renesas Electronics America can be found at www.renesas.com.

For more information, follow Renesas Electronics America at @RenesasAmerica on Twitter and http://www.facebook.com/RenesasAmerica.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする