2013年4月26日

KAWASAKI, JAPAN, SANTA CLARA, Calif., DUSSELDORF, Germany, April 26, 2013 — NLT Technologies (NLT), together with its sales and marketing channels in the Americas and Europe, Renesas Electronics America, Inc. and Renesas Electronics Europe GmbH, today announced the successful development of nine new mid-size color LCD modules with factory installed projected capacitive (PCAP) touch panel technology. The new LCD modules offer the increased durability, smooth operator interface, multi-touch functionality and clear image quality required for use in touch-panel displays designed for industrial applications, such as factory automation, test and measurement, as well as medical equipment. The nine new models are detailed below.

Diagonal Screen Size Resolution Part Number of Base LCD Module
6.5” (17cm) XGA (1024×768 pixels) NL10276BC13-01
VGA (640×480 pixels) NL6448BC20-30F
12.1” (31cm) XGA (1024×768 pixels) NL10276BC24-21
NL10276BC24-21F
15” (38cm) XGA (1024×768 pixels) NL10276BC30-39
NL10276BC30-34D
7.0” Wide (18cm) WVGA (800×480 pixels) NL8048BC19-02
NL8048BC19-02C
9.0” Wide (23cm) WVGA (800×480 pixels) NL8048BC24-09D

Total touch solution

NLT offers total PCAP solutions, that include the LCD, touch panel and controller board, direct from NLT’s factory. This is important for customers since the PCAP displays are covered by the same factory warranty NLT offers on all of their industrial LCD products. NLT also offers support for drivers and tuning software of touch panel, allowing customers to easily design NLT’s touch panel displays into their end products.

Long-term support same as Industrial LCD

NLT’s PCAP products offer the same long-term support program, high quality and Total Cost of Ownership (TCO) benefits as offered for their industrial LCD products.

Various PCAP Options

NLT’s PCAP touch panels offer valuable component and structural options such as bonding, surface treatment, or cover glass. This allows end product designers greater flexibility and more display options depending on the end use of the display.

Recently, the use of touch panel displays with multi-touch functionality is rapidly expanding in consumer applications like smart phones or tablet devices, as well as in industrial and medical applications. The increasing demand for PCAP touch panels continues due to their distinguished image quality, durability, and various construction design possibilities.

NLT Technologies continues to invest and develop new PCAP products and with the addition of the nine new products the PCAP family of products is now comprised of fourteen models in eight sizes. The company will continue to expand their touch panel product lineup as well as develop new applications for the company’s primary markets.

The new LCD modules will be showcased in NLT Technologies’ booth (#East 11-46) at Embedded System Expo, May 8-10, at Tokyo Big Sight in Japan, and also in Renesas Electronics America and NLT Technologies’ booth (#301) at Display Week 2013, May 21-23, at the Vancouver convention center in Canada.

Lineup of the PCAP modules can be found in the separate sheet.

About Renesas Electronics Europe’s Display Business

Renesas Electronics Europe is the authorized representative in Europe of NLT Technologies, Ltd. (established July 2011 as a joint venture between NEC Corporation and Shenzen AVIC Optoelectronics, Ltd.), a leading supplier of innovative LCD products for industrial applications. With an extensive lineup of 3.5- to 22.5-inch active-matrix LCD modules and a network of distributors, Renesas Electronics Europe provides complete display module solutions from NLT Technologies to the industrial, medical and high-end monitor market. In addition to modules based on NLT Technologies' SFT for ultra-wide viewing, Renesas Electronics Europe also offers LCD modules that include ultra-high resolutions, wide temperature ranges, high contrast ratios, rich color gamuts, backward compatibility, LED backlights, and transflective viewing for use in diverse lighting environments.

Renesas Electronics Europe and NLT Technologies are committed to delivering innovative, high-performance, eco-conscious LCD solutions that address the diverse size, power and high image-quality needs of their industrial, medical and high-end monitor customers. Based on technologies developed by NLT Technologies, the LCD modules are optimized and designed for a range of applications, including portable and fixed medical equipment, test and measurement devices, instrumentation equipment, point-of-sale systems, gaming systems, global positioning systems, factory automation and barcode scanners.

Additional information about these LCD display products, manufactured by NLT Technologies and represented by Renesas Electronics can be found at www.renesas.eu/display


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする