Intersil's Low Noise, Low Power Precision Amps, 24-Bit ADCs, Voltage Regulator, Combine With Renesas' Low Power MCU to Deliver Advanced Sensor Front End for Measuring Small Signals
2013年2月22日

MILPITAS, CA -- (MARKETWIRE) -- 02/22/13 -- Intersil Corporation (NASDAQ: ISIL), a leader in the design and manufacture of high-performance analog, mixed-signal and power management semiconductors, has joined with Renesas Electronics Corporation to develop a sensor signal conditioning solution for thermocouple, pressure and strain gauges. The companies will demonstrate the new solution, which is being distributed through Avnet Memec, at Embedded World February 26-28 in Nuremberg, Germany.

 

The pressure and strain gauge sensor signal conditioning designs use a combination of Intersil analog front ends coupled with a Renesas RL78/G13 microcontroller for extracting small sensor signals. Gain, filter, and digital conversion are completed then delivered to the RL78 MCU for further digital processing.

 

The Intersil-Renesas solution provides 24-bit low noise precision signal conditioning with a complete analog-to-digital front-end including the ISL28617, a low noise 40V instrumentation amplifier with integrated ADC driver, the ISL28134, a 5V low noise zero drift op amp, the ISL26102 24-bit delta sigma converter, and the ISL21090, an ultra low noise precision bandgap voltage reference, among others. Software interface is included for evaluation purposes.

 

The entire demo is powered from a debugger mini USB connection (or an optional 5V power supply) located on the Renesas RL78/G13 Demonstration Kit. The +12V, +10V, and ±5V supplies on the Intersil board are generated from the 3.3V supply on the Renesas board. The power supply design uses Intersil's ICL7660 voltage converter, ISL80138 linear regulator and ISL97516 step-up regulator.

 

Combining the low-power capabilities of Renesas' RL78 MCUs with Intersil's high-precision analog expertise provides customers with a complete solution to help bring applications to market quickly and efficiently. The new AFE-MCU solution is targeted toward industrial, medical and data acquisition applications. Each includes a sensor, signal conditioning circuits, and a Renesas microcontroller. Design engineers can review the reference design and evaluation platform for early prototype development at this URL: http://www.intersil.com/en/applications/signal-path-products/renesas.html

 

Intersil and the Intersil logo are trademarks or registered trademarks of Intersil Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

 


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする