2019年12月16日

SAN JOSE, Calif., December 16, 2019 – Integrated Device Technology, Inc. (IDT), a wholly-owned subsidiary of Renesas Electronics Corporation (TSE: 6723), announced today that it has been tasked by the City of Campbell, California, a city of 42,000 in the heart of California’s Silicon Valley, with making one of its parking lots “intelligent” as part of its efforts to be environmentally friendly, reduce light pollution, and make the lights more interactive for the city’s residents.

The effort began in June with four overhead lights in the City Hall’s employee parking lot and will soon expand to six additional overhead lights in the adjacent fenced Police Department parking lot. The project involved replacing the outdated sodium vapor bulbs with lamps comprised of much more energy-efficient and dimmable light emitting diodes (LEDs) and topping the lights with weather-proof 6LoWPAN wireless mesh network modules. These modules provide reliable connectivity to Campbell’s IT cloud infrastructure, giving the City’s IT staff complete control of the lights and enabling staff to monitor their operations continuously.

In addition to reducing the city’s energy usage, Campbell is actively considering using intelligent lighting in the City Hall parking lot. Locals have reportedly used the lot for private party transactions since the emergence of eBay, Craigslist, and other similar websites that allow private parties to advertise, buy, or sell merchandise. Smart lighting provides greater illumination by enabling this type of transaction to take place at night or in the early morning hours.

“The City of Campbell is the latest Silicon Valley city to recognize the numerous advantages of intelligent lighting, but they won’t be the last. There are literally millions of lights around  the world that can be quickly and easily converted into intelligent lighting at a low cost, while also providing a far more energy-efficient solution with more advanced capabilities,” said Rudi Hechfellner, director of sensing technology at IDT. “Our comprehensive lines of sensor, wireless networking, power and timing devices make IDT an ideal source when developing intelligent lighting, smart city, and other IoT-related applications.”

Based on their current experience, the City is considering giving their intelligent lights additional capabilities, such as automatically turning on when people approach the area. This would be accomplished by the lights using advanced artificial intelligence (AI) algorithms to discriminate between people, animals, and vehicles – even in low light conditions – rather than relying on the cloud. This approach ensures that lights provide illumination immediately rather than experiencing a delay, as data is first transmitted to the cloud for processing, and an activation signal is eventually sent. Also, multiple lights could communicate with each other in the areas, so that each illuminates and dim precisely to ensure a pedestrian is always well lit while walking. Such intelligence is a significant advance over simple motion sensors, enabling lights to provide continuous illumination for people even when they are not moving, such as sitting at a bus stop, for example.

Visit the lighting webpage to learn more information about IDT’s smart lighting solutions.

About IDT

Integrated Device Technology, Inc., a wholly-owned subsidiary of Renesas Electronics Corporation (TSE: 6723), develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, high-performance timing, memory interface, real-time interconnect, optical interconnect, wireless power, and smart sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities, and distribution partners throughout the world. Additional information about IDT can be found at www.IDT.com. Follow us on Facebook, LinkedIn, Twitter, and YouTube.

###

©2019, Integrated Device Technology, Inc. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. and its worldwide subsidiaries. All other brands, product names, and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

この記事をシェアする